cancel
Showing results for 
Search instead for 
Did you mean: 

CAN-Bus no callback/received frame; FDCAN STM32G474

Hello,

when I try to receive a CAN-Frame it is not received by the Microcontroller, it is within the range, I have no idea what the issue is.

Thanks to everybody in advance, Best Regards, Seppel

0693W00000bhUdqQAE.png0693W00000bhUe5QAE.png 

0693W00000bhUeFQAU.png 

void FDCAN_Config(FDCAN_HandleTypeDef *pHfdcan)
{
 
    pHandleToFdCan = pHfdcan;
 
  /* Configure Rx filter */
  sFilterConfig.IdType = FDCAN_STANDARD_ID;
  sFilterConfig.FilterIndex = 0;
  sFilterConfig.FilterType = FDCAN_FILTER_RANGE;
  sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
  sFilterConfig.FilterID1 = 0x700;
  sFilterConfig.FilterID2 = 0x7FF;
  if (HAL_FDCAN_ConfigFilter(pHandleToFdCan, &sFilterConfig) != HAL_OK)
  {
    Error_Handler();
  }
 
  /* Configure global filter:
     Filter all remote frames with STD and EXT ID
     Reject non matching frames with STD ID and EXT ID */
  if (HAL_FDCAN_ConfigGlobalFilter(pHandleToFdCan, FDCAN_REJECT, FDCAN_REJECT, FDCAN_REJECT, FDCAN_REJECT) != HAL_OK)
  {
    Error_Handler();
  }
 
 
 
  /* Start the FDCAN module */
  if (HAL_FDCAN_Start(pHandleToFdCan) != HAL_OK)
  {
    Error_Handler();
  }
 
  if (HAL_FDCAN_ActivateNotification(pHandleToFdCan, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK)
  {
    Error_Handler();
  }
 
}

0693W00000bhUf3QAE.png 

P.S. TX works perfectly fine, as you can see it Ack's the 0x701 Frame that was received.

22 REPLIES 22

Yes, the RX callback is working fine.

Here's my setup. In this case for an H7 MCU. Bitrate is 500kB

static void MX_FDCAN1_Init(void)
{
 
  /* USER CODE BEGIN FDCAN1_Init 0 */
 
  /* USER CODE END FDCAN1_Init 0 */
 
  /* USER CODE BEGIN FDCAN1_Init 1 */
 
  /* USER CODE END FDCAN1_Init 1 */
  hfdcan1.Instance = FDCAN1;
  hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
  hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
  hfdcan1.Init.AutoRetransmission = DISABLE;
  hfdcan1.Init.TransmitPause = DISABLE;
  hfdcan1.Init.ProtocolException = DISABLE;
  hfdcan1.Init.NominalPrescaler = 4;
  hfdcan1.Init.NominalSyncJumpWidth = 8;
  hfdcan1.Init.NominalTimeSeg1 = 12;
  hfdcan1.Init.NominalTimeSeg2 = 2;
  hfdcan1.Init.DataPrescaler = 10;
  hfdcan1.Init.DataSyncJumpWidth = 1;
  hfdcan1.Init.DataTimeSeg1 = 13;
  hfdcan1.Init.DataTimeSeg2 = 2;
  hfdcan1.Init.MessageRAMOffset = 0;
  hfdcan1.Init.StdFiltersNbr = 0;
  hfdcan1.Init.ExtFiltersNbr = 0;
  hfdcan1.Init.RxFifo0ElmtsNbr = 1;
  hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;
  hfdcan1.Init.RxFifo1ElmtsNbr = 1;
  hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;
  hfdcan1.Init.RxBuffersNbr = 10;
  hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8;
  hfdcan1.Init.TxEventsNbr = 10;
  hfdcan1.Init.TxBuffersNbr = 2;
  hfdcan1.Init.TxFifoQueueElmtsNbr = 2;
  hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
  hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_8;
  if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN FDCAN1_Init 2 */
  /* USER CODE END FDCAN1_Init 2 */
 
}

After calling the above init in my main, I call these two:

 if (HAL_FDCAN_Start(&hfdcan1) != HAL_OK)
    {
      Error_Handler();
    }
	if(HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK)
    {
      Error_Handler();
    }

When any CAN message is sent by a node other than the ST MCU, this callback is triggered:

void HAL_FDCAN_RxFifo0Callback(FDCAN_HandleTypeDef *hfdcan, uint32_t RxFifo0ITs)
{
	 if (HAL_FDCAN_GetRxMessage(hfdcan, FDCAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK)
	    {
	    Error_Handler();
	    }
	 if (RxHeader.Identifier==0x250)		 PC13state++;
}

LCE
Principal II

And in the IRQ handler I check its source, set some flags which I check later in main, then call the HAL IRQ handler to reset register flags.

/**
  * @brief This function handles FDCAN1 interrupt 0.
  */
void FDCAN1_IT0_IRQHandler(void)
{
	/* get PTP time */
	ETH_PTPTime_GetTime(&sTimeCanRx);
 
	if( FDCAN1->IR & FDCAN_IR_RF0N )
	{
		sCan1RxFifo0.RxdIrq = 1;
		sCan1RxFifo0.sTimeRx.seconds = sTimeCanRx.seconds;
		sCan1RxFifo0.sTimeRx.nanosec = sTimeCanRx.nanosec;
	}
	if( FDCAN1->IR & FDCAN_IR_RF1N )
	{
		sCan1RxFifo1.RxdIrq = 1;
		sCan1RxFifo1.sTimeRx.seconds = sTimeCanRx.seconds;
		sCan1RxFifo1.sTimeRx.nanosec = sTimeCanRx.nanosec;
	}
	if( FDCAN1->IR & FDCAN_IR_DRX )
	{
		sCan1RxBuffer.RxdIrq = 1;
		sCan1RxBuffer.sTimeRx.seconds = sTimeCanRx.seconds;
		sCan1RxBuffer.sTimeRx.nanosec = sTimeCanRx.nanosec;
	}
 
	HAL_FDCAN_IRQHandler(&hCan1);
}

Hello,

the issue is resolved:

Issue visible in the Code:

hfdcan2.Init.StdFiltersNbr = 0;

Solution, change the Config in the Stm32CubeIde, set the number of filters to 1, the generated code will be:

hfdcan2.Init.StdFiltersNbr = 1;

Thanks a lot to everybody supporting the case.

Best Regards, Seppel

P.S. It is so obvious that if you use a filter the number of filters should not be zero. But as always: "You know afterwards, what you could have known in advance". 8)