2020-01-23 2:44 AM
Using Project Manager -> Advanced Settings -> Generated Function Calls you can change the initialization order. However this setting is ignored when writing the code.
You have to manually change the order in the .ioc file in this line:
ProjectManager.functionlistsort=1-MX_GPIO_Init-GPIO-false-HAL-true,2-SystemClock_Config-RCC-false-HAL-false,3-MX_DMA_Init-DMA-false-LL-true,4-MX_LPUART1_UART_Init-LPUART1-false-LL-true,5-MX_TIM20_Init-TIM20-false-LL-true,6-MX_USART3_UART_Init-USART3-false-HAL-true,7-MX_ADC1_Init-ADC1-false-LL-true,8-MX_ADC2_Init-ADC2-false-LL-true,9-MX_ADC3_Init-ADC3-false-LL-true,10-MX_ADC4_Init-ADC4-false-LL-true,11-MX_ADC5_Init-ADC5-false-HAL-true
Changing the numbers is what CubeMX is doing, but that is not enough. You have to actually reorder the items.
CubeIDE:
Version: 1.2.1
Build: 5190_20200115_1224 (UTC)
STM32CubeG4 Firmware Package V1.1.0 / 28-June-2019
Solved! Go to Solution.
2020-01-24 4:20 AM
This was reported in another thread and I wrote a ticket about it at that time. It will be fixed in an upcoming release.
2020-01-24 4:20 AM
This was reported in another thread and I wrote a ticket about it at that time. It will be fixed in an upcoming release.
2021-07-21 2:33 PM
@Markus GIRDLAND
For what it's worth, this is still happening to me as of today using STM32CubeIDE 1.7.0 with a STM32F030C8T.
Spent hours trying to figure out what I had done wrong.