Question
Why is code generated for analog watchdogs 2 & 3 if ADC sequencer is set to not fully configurable?
- March 25, 2025
- 3 replies
- 676 views
Newcomer to CubeIDE. When I set the ADC parameters for fixed sequencing, i.e. not fully configurable, some initialization code is generated for watchdogs 2 & 3 (see below). I don't want to use analog watchdogs or have to edit the main.c file manually. Is this a bug, or is there some way to alter this behaviour? Only watchdog 1 seems to have an enable check box.
I'm using STM32CubeIDE Version: 1.18.0, Build: 24413_20250227_1633 (UTC) on Linux.
/** Configure the WatchDogs 2
*/
AnalogWDGConfig.WatchdogNumber = ADC_ANALOGWATCHDOG_2;
AnalogWDGConfig.WatchdogMode = ADC_ANALOGWATCHDOG_SINGLE_REG;
if (HAL_ADC_AnalogWDGConfig(&hadc1, &AnalogWDGConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure the WatchDogs 3
*/
AnalogWDGConfig.WatchdogNumber = ADC_ANALOGWATCHDOG_3;
if (HAL_ADC_AnalogWDGConfig(&hadc1, &AnalogWDGConfig) != HAL_OK)
{
Error_Handler();
}