2024-10-09 06:19 PM
Hi i'm using MCU : STM32H743ZGT.
At several ADC documents, it says that when ADC1 and ADC2 end sampling, the two results are stored in ADC_CDR together.
The top 16 bits are the result of ADC2, or slave ADC, and the bottom 16 bits are the result of ADC1, or master ADC.
I want to know how the two ADCs are stored in different registers, for example, each ADC_DR.
Because I want to get more than 16 bits of data.
Of course, we use the two ADCs as dual mode.
Is there any other way?
Thank you.