STM32CubeMonitor (MCUs)

Ask questions on STM32CubeMonitor. Discuss the latest updates, including specialized versions (power, RF, USB-PD).

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMonitor-1.12.0 is available

Hello The version 1.12.0 of STM32CubeMonitor is available on st.com :  https://www.st.com/en/development-tools/stm32cubemonitor.html What are the main changes in this version ? Node-RED® updated to version 4.1.3.STM32 devices list updated.Software de...

STM32CubeMonitor-RF V2.19.0 is available

Hello A new release of STM32CubeMonitor-RF is available on st.com. Click on "Get latest" to download the version 2.19.0. What are the main changes in this version ? Alignment with STM32CubeWB firmware 1.24.0.Alignment with STM32CubeWBA firmware 1.8.0...

Resolved! How can I add additional nodes?

I have STM32CubeMonitor v1.4.0 installed on my home computer and work computer.On my home computer, there is an option called "Manage Palette" which allows me to add additional nodes from nodered online resourcesOn my work coputer, there is no such o...

0693W00000VOcqWQAT.png 0693W00000VOcqbQAD.png

My chart crashes, I want the chart to only display the data of the last 30s, and the rest of the data is not needed. I'm testing the timestamp is achievable, but it won't work on the serial port.

This is a serial input, the data volume per second is 12000bytes (1k Sampling rate*4channel*3bytes (single-channel sampling data size)). The input content of the serial port is as follows (part of the picture is intercepted) :serial port output forma...

0693W00000WICyMQAX.png
Lep by Senior
  • 864 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeMonitor 1.4.0 CPU critical performance issue

Hello everyone.I'm trying to work with STM32CubeMonitor to implement an industrial machine Life Test JIG using 12 ST-LINK v2 probes connected to STM32 microcontrollers by SWD protocol, but I'm facing very strange and anoying issues.This post will foc...

0693W00000Kdj6MQAR.png 0693W00000Kdj75QAB.png 0693W00000Kdj8NQAR.png
acv_atr by Associate III
  • 5141 Views
  • 14 replies
  • 0 kudos

Resolved! STM32CubeMonitor Security/Credentials critical issues

Hi everyone.I'm trying to secure STM32CubeMonitor Editor and UI as defined to Node-RED, but is not possible secure STM32CubeMonitor.After define a user and password at settings.js (even only for STM32 CubeMonitor) the editor and UI breaks and are sim...

0693W00000KdjWjQAJ.png 0693W00000KdjVcQAJ.png 0693W00000KdjXFQAZ.png
acv_atr by Associate III
  • 3916 Views
  • 10 replies
  • 0 kudos