cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMonitor cannot start monitoring on Linux when running as normal user.

drid
Associate II

Console displays error [warn] OS priority setting: SystemError [ERR_SYSTEM_ERROR]: A system error occurred: uv_os_setpriority returned EACCES (permission denied)

Within the application these errors occur hen pushing start:

Bad parameter (7)

Bad parameter (7): start

When run with sudo, error does not appear and monitor works as it should

Ubuntu 21.04 installed from deb file

1 ACCEPTED SOLUTION

Accepted Solutions
Richard.Chvr
ST Employee

Hello @drid​ 

Warning has been corrected in the latest 1.4.0 release of STM32CubeMonitor.

do you still face Bad parameter issue?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Richard.Chvr
ST Employee

Hello @drid​ 

Warning has been corrected in the latest 1.4.0 release of STM32CubeMonitor.

do you still face Bad parameter issue?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.