STM32CubeMonitor (MCUs)

Ask questions on STM32CubeMonitor. Discuss the latest updates, including specialized versions (power, RF, USB-PD).

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMonitor-1.12.0 is available

Hello The version 1.12.0 of STM32CubeMonitor is available on st.com :  https://www.st.com/en/development-tools/stm32cubemonitor.html What are the main changes in this version ? Node-RED® updated to version 4.1.3.STM32 devices list updated.Software de...

STM32CubeMonitor-RF V2.19.0 is available

Hello A new release of STM32CubeMonitor-RF is available on st.com. Click on "Get latest" to download the version 2.19.0. What are the main changes in this version ? Alignment with STM32CubeWB firmware 1.24.0.Alignment with STM32CubeWBA firmware 1.8.0...

Resolved! Get exefile parameter from "variables"-node

Hello,I'm using the current version of STM32CubeMonitor (1.6.0) under Windows and would like to check in my flow if the configured exefile in the STMicroelectronics variable node is the intended one (e.g fits a regex). For this I would like to read o...

MKori.1 by Associate III
  • 2721 Views
  • 3 replies
  • 0 kudos

STM32CubeMonitor stuck at 10% when parsing .elf

When compiling with Maximum (-g3) Debug level, Add new exe-config config mode stalls at 10% when loading .elf. Why is this? Is there a limit to the number of symbols or the size of the .elf?If compiled with Default (-g) Debug level, then loads OK.Whe...

_kj_ by Associate
  • 1276 Views
  • 1 replies
  • 0 kudos

STM32CubeMonPwr for Linux

Hi, Does anybody has a problem with latest version (1.2.1) of the STM32CubeMonPwr software? Looks like Linux archive is broken. I tried to fix it but without any success.  

stm cube monitor

Im trying to use a switch button to control a Boolean variable, but i couldn't find a way to make it work. If anyone know what i need to connect to it and to define i will be thankful.       

Yifatdvir_2-1692510196328.png

stm cubemonitor power v1.2.1

a)On windows 11 with 2 screen the cubemonitor power v1.2.1 starts on one screen with the size way bigger than the screen. I have to resize the windows on the left outer edge -> height shrink automatically to match screen size -> then can move the who...

_richard by Associate III
  • 1193 Views
  • 0 replies
  • 0 kudos