Skip to main content
TLIM.2
Visitor II
April 1, 2023
Solved

[STM32Cube Monitor] Can't write data of variables in Write panel node

  • April 1, 2023
  • 1 reply
  • 1674 views

Data is showing properly in Chart node but can't write data with write panel widget0693W00000bhKsHQAU.jpg. When I try this work after change target board ( before : STM32F407G-DISC1 --> after : EVSPIN32F0601S1) the problem was resolved. I would like to know what is the difference between that two boards for working of "Write panel node". Please help me...

This topic has been closed for replies.
Best answer by Richard.Chvr

Hello @TLIM.2​ 

There's no difference in between both boards, Write node does not check the connected board. Need to check whether your y variable address and executable file are correct in STM32F407G case.

You can also try to write variable through a variable flow, see wiki and check in that case if it work or not.

1 reply

Richard.Chvr
Richard.ChvrBest answer
ST Technical Moderator
April 6, 2023

Hello @TLIM.2​ 

There's no difference in between both boards, Write node does not check the connected board. Need to check whether your y variable address and executable file are correct in STM32F407G case.

You can also try to write variable through a variable flow, see wiki and check in that case if it work or not.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.