STM32CubeMonitor (MCUs)

Ask questions on STM32CubeMonitor. Discuss the latest updates, including specialized versions (power, RF, USB-PD).

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMonitor-1.12.0 is available

Hello The version 1.12.0 of STM32CubeMonitor is available on st.com :  https://www.st.com/en/development-tools/stm32cubemonitor.html What are the main changes in this version ? Node-RED® updated to version 4.1.3.STM32 devices list updated.Software de...

STM32CubeMonitor-RF V2.19.0 is available

Hello A new release of STM32CubeMonitor-RF is available on st.com. Click on "Get latest" to download the version 2.19.0. What are the main changes in this version ? Alignment with STM32CubeWB firmware 1.24.0.Alignment with STM32CubeWBA firmware 1.8.0...

Resolved! CubeMonitor doesn't understand 'bool' types

Trying to monitor a 'C' variable of type bool results in the errornot connected ! bad parameter (7)and the probe connection drops. It then comes back all on its own!!Changing the variable to any other type and the monitor runs fine.

Resolved! Bad Installation on Windows 7

Helo, Dear ST!I very happy for use Yours many devices. They are very cool! You are very cool too!So, I was download Your STM32Monitor on my PC. But after install this software on the my Windows 7 I seen unreal picture:Installator of STM32Monitor putt...

ATim.1 by Associate
  • 1254 Views
  • 2 replies
  • 0 kudos

Resolved! Conditional Data Logging

I want to in corporate conditional data logging in Cube Monitor Flow, since i intend to monitor the behaviour over many hours.My requirement is to log all the 4 fields:ms_enDeviceOrientationms_stStAccelDataXms_stStAccelDataYms_stStAccelDataZonly if m...

VOlet.1 by Associate II
  • 5355 Views
  • 11 replies
  • 0 kudos

Resolved! STM32CubeMonitor looses some variable selections on Edit

After rebuilding an ELF file, going into the Edit Variables node indicates that those variables alphabetically near the top are retained but those further down the list have been dropped requiring them to be re-selected. Is this a memory overflow and...

Resolved! Data plot of MCU Memory

Hi Everyone!​I just started my first STM32F4 project and I was wondering if there is an IDE that can show the content of a range of memory in form of a data plot.​I ​tried to find someting on the web but had no luck so far.​This means for debug I am ...

Cde.1 by Associate
  • 2483 Views
  • 4 replies
  • 0 kudos

STM32 Monitor with B-STLINK-ISOL V3

I'm having trouble monitoring signals of my project running on an STM32G431 through STLINK-V3SET and B-STLINK-ISOL. The system works well with the STLINK-V3SET alone.Regarding link settings on the STLINK-V3SET and B-STLINK-ISOL: I've removed JP1 on t...

SW-Mark by Associate
  • 1133 Views
  • 0 replies
  • 0 kudos