2023-04-14 5:36 AM
Good morning! I have a problem with the STM32F429I-DISC1 board. I bought this board a few weeks ago and with the STMCubeIde software (v. 1.12.0) I downloaded the BSP example for this board together with the STM32CubeF4 package (v. STM32Cube_FW_F4_V1.27.0). After compiling the project and loading it into the board (Run as STM32 C/C++ Application), the execution hangs during the calibration of the touch-screen (activate the colored circle inside the rectangle). I tried with various PCs with Windows 10 Pro (I7 and I5 with 16 GB of RAM) and also on a Linux Kubuntu v.22.04 machine but the anomaly always occurs. Another example (LTDC_Display_2Layers) works correctly. I also tried to use another STM32F429I-DISC1 card but the problem remains. Can anyone enlighten me on this? Thank you!
2023-04-14 5:44 AM
> execution hangs
How exactly? Where is the PC in debugger?
JW
2023-04-14 5:52 AM
The pc is an I7 Intel (motherboars Asus Prime Z270A - Processor Intel(R) Core(TM) i7-6700 CPU @ 3.40GHz 3.41 GHz with 16 GB Kingston)
2023-04-14 6:01 AM
The execution of the software stops when the colored circles to press appear. Despite pressing with my finger or with a touch-pen, the circles do not color and freeze. I just have to reset:
2023-04-24 8:27 AM
Hello Alann ,
This BSP example configuration has been running on STMicroelectronics STM32F429I-Discovery RevC board, and in order to run it on STMicroelectronics STM32F429I-Discovery RevD or RevE boards (NB: check your board revision ) , please ensure to add "USE_STM32F429I_DISCOVERY_REVD" define in the toolchain's pre-processor options and download the update fix form github : Update touch calibration to fix inverted touch panel on STM32F429I-DI… · STMicroelectronics/STM32CubeF4@d7fef24 · GitHub
Br
Moez
2023-04-25 8:56 AM - edited 2023-11-20 8:10 AM
Good morning and thank you! How do I see the REV of the card? I don't see any indication on the circuit board.
Aldo
2023-04-25 9:26 AM - edited 2023-11-20 8:11 AM
Hi Alann ,
as mentioned on the picture below , your board is STM32F429I-Discovery RevE.
Br
Moez
2023-04-25 9:50 AM
PC = Program Counter
If you stop execution in the debugger, where in the whole of the code is it sitting / stuck.
ie while(1) loop in HardFault_Handler() or Error_Handler(), or some other place that can be identified..
2023-04-26 12:49 AM
Good morning! I made the suggested corrections and the circles are colored regularly...thanks. But it hangs up after another error: MEM$ - cannot be initialized. So I need more suggestions. Thanks again.
2023-04-27 2:34 AM
Hello Alann ,
Could you please provide more details : at which level exactly is the error faced? If at compilation level, which IDE are you using? did you add this modification under this path : Drivers/BSP/STM32F429I-Discovery/stm32f429i_discovery_ts.c ?
if defined (USE_STM32F429I_DISCOVERY_REVD)
if (y > 3700)
{
y = 3700;
}
else if (y < 180)
{
y = 180;
}
/* Y value first correction */
y -= 360;
y = 3700 - y;
#else
/* Y value first correction */
y -= 360;
#endif
and please add "USE_STM32F429I_DISCOVERY_REVD" define in the toolchain's pre-processor options ,
Br
Moez