2024-08-03 11:23 AM
Hello,
I updated to Mac15 (MacOS Sonoma Public Beta), which was probably a mistake. Now I get an error from STMCubeIDE when I try to run indicating "ST-Link Server is required to launch the debug session" and to Please download it on www.st.com.
I figured something changed in the OS that no longer makes the ST-Link Server run any more.
However when I try to download it, I get essentially a broken link, or at least it simply wont download. Even worse, the web page with Safari seems entirely broken and I cant even get a download to start after accepting the license, but with FireFox I get further, I get but still wont download and the link seems broke.
I can still flash using the STM32CubeProgrammer fortunately (using 2.13.1).
Can anyone tell me how to download this ST-Link Server? Or if there is an issue with the last MacOS and this and there is no fix?
Solved! Go to Solution.
2024-11-13 10:03 AM
this solution does't worked for me
2024-11-13 11:21 AM
Can you please check this way?
https://community.st.com/t5/stm32cubeide-mcus/stlink-server-with-macos-15/m-p/741051/highlight/true#M32168
2024-11-14 03:01 AM - edited 2024-11-14 08:23 AM
Thank you
2024-11-14 03:26 AM
Hi there, the sudo command doesn't work for me, have you found another solution?
2024-11-14 05:25 AM
this way doesn't work
2024-11-14 05:31 AM
Hmmm.
This might be due to running with the sudo command. It could have broken some permissions.
2024-11-14 06:08 AM
In fact it now works - but I am using a French keyboard and using sudo, it is seen as a UK one and I cant switch back.
Inconvenient but at least I am not stuck.
Thanks for your help
2024-11-14 06:08 AM
Exactly the same here - I cannot revert to my French keyboard.