2024-04-05 07:32 AM - last edited on 2025-02-07 12:22 AM by SofLit
I have an H755ZL and so I downloaded CubeIDE and CubeMX to begin familiarizing myself. I am unable to install the cubeMX H7 package so I cannot generate any code for my MCU. In either CubeIDE or CubeMX when I go to "manage embedded software" nothing happens. I also cannot login as nothing happens when I click that either.
Solved! Go to Solution.
2024-04-09 04:11 AM - edited 2024-04-09 04:12 AM
Hello @christophersmith1618 ,
CubeIDE is only supported for Windows 10 and 11. So, using Windows 7 might affect the IDE functionality.
Thanks,
Rim.
2024-04-05 07:38 AM
Hello and welcome to the community.
Could you please share warning or error messages you are facing?
2024-04-05 08:15 AM
There are no warning or error message, no messages of any kind. When I click on the selection in the drop down nothing happens.
2024-04-05 08:21 AM - edited 2024-04-05 08:22 AM
Ok not sure I understood the issue.
Do you mean when you want to select "Manage Software Packs" from "Software Packs" menu nothing happens?
In fact this window should show up:
2024-04-05 08:23 AM
Yes that is exactly what I mean
2024-04-05 08:25 AM - edited 2024-04-05 08:26 AM
Did you try to uninstall/install CubeMx?
Could you please provide the version of CubeMx? which platform?
2024-04-05 08:28 AM
I just downloaded CubeMX and CubeIDE so they are the latest versions. I have not tried uninstalling yet. I am on windows 7
2024-04-05 08:30 AM
Try to uninstall/install it and get back to us with the results.
2024-04-05 01:56 PM
This may or may not be the issue, but Windows7 has not been supported since some time before CubeMX version 6.2 (March 2021). It was supported in CubeMX 5.6, and I don't have any release notes for versions between 5.6 and 6.2.
2024-04-05 03:18 PM
@Semer CHERNI could confirm this point.