Hello @Alexmouse and welcome to the community,
In the attached screenshot there are two main files open, so make sure that the code where you are trying to set the breakpoint is actually being executed. Also check that compiler optimisations are o...
Hello @Saranya_2003 ,
Could you please try these points:
Check that STLinkServer is installed or install it from this site.When you plug the board to the PC, It should enumerate as a STLink debug probe in device manager.Upgrade STLink firmware.Chec...
Hello @chris1seto and welcome to the community,
The problem is not reproduced with the latest version of CubeIDE. Could you specify which CubeIDE you are working with?
Thanks,
Rim.