2020-06-25 6:27 AM
Hello. When I press to Run (Run main.c) button, STM32CubeIDE opens random file, possibly, from current repository, for example: startup_stm32l452xx.s, core_cm4.h etc...
Code is loading successful, but this side effect bothers me.
I would like to disable this function. How can I do it?
If you need more information about this behavior please, ask.
Thank you for reading.
Solved! Go to Solution.
2024-11-06 7:29 AM - edited 2024-11-06 7:29 AM
Only now I noticed that 'Run' button indeed flips from incactive to active during flashing process/debug session launch, but I am not able to click it as there is a modal window showing progress of the flashing progress
Maby I enabled that modal progress window somewhere.
2024-11-06 7:34 AM
Hm, so this thread started in 2020, 1.14 was released in 2023. Where can I see release dated of CubeIDE versions ?
What Cube version was 'the latest' in 2020 ?
I do not see release dates for each release in Release Note
https://www.st.com/resource/en/release_note/rn0114-stm32cubeide-release-v1161-stmicroelectronics.pdf
2024-11-06 7:34 AM
@ferro wrote:Only now I noticed that 'Run' button indeed flips from incactive to active during flashing process/debug session launch, but I am not able to click it as there is a modal window showing progress of the flashing progress
I'm using STM32CubeIDE 1.15.1 at the moment, I haven't seen the window. I also have external flash which flashes after the internal flash is flashed and that can take a while. Most of the time I can control myself to not press the button, but it's so tempting to click a green play button that I sometimes forget.
2024-11-06 7:36 AM
"it's so tempting to click a green play button" haha, I know, hard to resist el ou el
2024-11-06 11:21 AM - edited 2024-11-06 11:21 AM
There is a kind of information about release dates but would rather see it stated within each version update note. not as a sideproduct of the document's revision history.
So this thread started on Jun 2020, when CubeIDE latest version was 1.3.1.
https://www.st.com/resource/en/release_note/rn0114-stm32cubeide-release-v1161-stmicroelectronics.pdf
2024-11-07 4:24 AM
>> "I haven't seen the window"
You will with this option off:
[Debug Configurations > Common]
2024-11-07 6:29 AM - edited 2024-11-27 6:14 AM
There are currently several topics open on this problem:
I work with STM32CubeIDE daily and it is one of my main annoyances.
All I want from my IDE is not to open files unless there is a breakpoint. Is that too much too ask?
2024-11-27 5:51 AM
The problem still exists in 1.17.0
As this case is incorrectly marked as solved, I opened a new one for 1.17.0:
I will keep doing it for every new release, until it is fixed, or I drop dead - whichever comes first.