cancel
Showing results for 
Search instead for 
Did you mean: 

I2C communication between STM32L4R5 and esp32

ejeee
Associate

I tried creating I2C connection between my stm32 board and esp32. I assume it is not working because of my code, due to the wiring being so simple in I2C communication, the pull up resistor is connected externally. Do you guys see any mistake in my code that could make my I2C to not work?  I cannot figure out why it would not work.

9 REPLIES 9
Hl_st
ST Employee

Hello,

there seems to me two potentially problems. At first, there should be connected pull up resistor to both I2C pins (SDA and SCL). The second, you are shifting slave address 0x08 in: 

HAL_I2C_Master_Receive(&hi2c2, 0x08 << 1, &receivedByte, 1, 100)

 I would say, there should be:

HAL_I2C_Master_Receive(&hi2c2, 0x08, &receivedByte, 1, 100)

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


@Hl_st wrote:

Hello,

there seems to me two potentially problems. At first, there should be connected pull up resistor to both I2C pins (SDA and SCL). The second, you are shifting slave address 0x08 in: 

HAL_I2C_Master_Receive(&hi2c2, 0x08 << 1, &receivedByte, 1, 100)

 I would say, there should be:

HAL_I2C_Master_Receive(&hi2c2, 0x08, &receivedByte, 1, 100)

 


Being that the slave address is 0x08 on the ESP32, then the OP is correct in shifting the slave address 0x08 left by 1 as indicated in the comments ST provides.

/**
  * @brief  Transmits in master mode an amount of data in blocking mode.
  * @PAram  hi2c Pointer to a I2C_HandleTypeDef structure that contains
  *                the configuration information for the specified I2C.
  * @PAram  DevAddress Target device address: The device 7 bits address value
  *         in datasheet must be shifted to the left before calling the interface
  * @PAram  pData Pointer to data buffer
  * @PAram  Size Amount of data to be sent
  * @PAram  Timeout Timeout duration
  * @retval HAL status
  */
HAL_StatusTypeDef HAL_I2C_Master_Transmit(I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint8_t *pData,
                                          uint16_t Size, uint32_t Timeout)
{
  uint32_t tickstart;
  uint32_t xfermode;

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

OK, I wasn´t sure how it is on ESP32 <--> STM32 communication, but for STM32 <--> STM32 communication address shouldn´t be shifted.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


@ejeee wrote:

 I assume it is not working because of my code, .


Don't just jump to that conclusion!

First, use an oscilloscope to what - if anything - is happening on the wires.

It could very well be a hardware problem.

That's why you need to show the schematics of your setup - see: How to write your question to maximize your chances to find a solution.

 


@ejeee wrote:

I tried creating I2C connection between my stm32 board and esp32. 


So which one is the Master, and which is the slave?

  • Have you tested your Master against a standard, well-known, known-working Slave?
  • Have you tested your Slave against a known-working Master?

Don't make the classic mistake of trying to do both ends of the link at once:

https://community.st.com/t5/stm32-mcus-products/i2c-communication-between-two-different-stm32-evk-boards/m-p/755042/highlight/true#M268963

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hello,

Thank you for your advice! I did try to look at the SCL line, it shows some kind of square wave. But it seems there are a lot of noise of some sort in the SCL line. I do not have access to an oscilloscope at the moment. But, I will post my findings soon. 

Let's say I do not have access to the I2C Demo Board, what other way should I test my master and slave? Thanks for your help.

There are loads of low-cost "breakout" boards for common I2C devices...

AndrewNeil_0-1738248543073.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@Hl_st wrote:

OK, I wasn´t sure how it is on ESP32 <--> STM32 communication, but for STM32 <--> STM32 communication address shouldn´t be shifted.


That is incorrect about the STM32<>STM32. With the HAL driver, you MUST shift the slave address. That is one of the quirks of the ST's HAL I2C driver. All other companies' I2C drivers does that automatically for you.

 

You are forgetting about the read bit, which is set at bit 0 position. The slave devices parses the upper 7 bits for the slave address and bit 0 for the read flag. 

 

Think about a slave device with a slave address set as 0x09. If the master wants to read from that slave device, and without shifting, it'll send 0x09 on the bus. But the slave device will see the slave address as 0x04, not 0x09. 

And if you want to write to the slave, the master will send 0x09 on the bus, but bit 0 is set, which is a read flag, not a write.

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.

@Karl Yamashita wrote:


 All other companies' I2C drivers does that automatically for you..


That's not true.

Sadly, there is inconsistency & confusion throughout the industry - both in hardware documentation, and software implementations.

https://www.avrfreaks.net/s/topic/a5C3l000000UZ4wEAG/t148636?comment=P-1418813 

https://www.avrfreaks.net/s/topic/a5C3l000000UcHrEAK/t160967?comment=P-1322043

https://www.avrfreaks.net/s/topic/a5C3l000000Ua6EEAS/t152560?comment=P-1244847

https://www.avrfreaks.net/s/topic/a5C3l000000UXMPEA4/t142031?comment=P-1150738

etc, etc, etc, ...

 

PS:

@ejeee  The ST HAL documentation is pretty clear on this:

/**
  * @brief  Checks if target device is ready for communication.
  * @note   This function is used with Memory devices
  * @param  hi2c Pointer to a I2C_HandleTypeDef structure that contains
  *                the configuration information for the specified I2C.
  * @param  DevAddress Target device address: The device 7 bits address value
  *         in datasheet must be shifted to the left before calling the interface
  * @param  Trials Number of trials
  * @param  Timeout Timeout duration
  * @retval HAL status
  */
HAL_StatusTypeDef HAL_I2C_IsDeviceReady( I2C_HandleTypeDef *hi2c, uint16_t DevAddress, uint32_t Trials, uint32_t Timeout )

 The I2C Slave address is 7 bits:

+----+----+----+----+----+----+----+
| A6 : A5 : A4 : A3 : A2 : A1 : A0 |
+----+----+----+----+----+----+----+

 You present that to the HAL in a byte as:

+----+----+----+----+----+----+----+----+
| A6 : A5 : A4 : A3 : A2 : A1 : A0 : 0 |
+----+----+----+----+----+----+----+----+

(well, strictly, you pass it in a uint16_t where the top byte is all zeros)

 

The documentation for the Arduino Wire I2C library says,

"Note: There are both 7 and 8-bit versions of I2C addresses"

That's not strictly true - The I2C Specification clearly defines the Slave Address to be bits.

What they mean is that many sources will (incorrectly) use "I2C address" to mean the combination of both the actual Address (7 bits) and the R/W bit.

The Arduino documentation goes on to say:

"7 bits identify the device, and the eighth bit determines if it’s being written to or read from."

Which is true.


This is a clue: If you see anything which talks about a slave having two addresses (one for read, one for write, which differ by just 1 in the LSB) then they are talking about the combination of Address + R/W bit.


The Arduino documentation further says: 

"The Wire library uses 7 bit addresses throughout. If you have a datasheet or sample code that uses 8-bit address, you’ll want to drop the low bit (i.e. shift the value one bit to the right), yielding an address between 0 and 127."

In other words, when you pass the Address to the Wire library, it must be like this:

+----+----+----+----+----+----+----+----+
| 0 | A6 : A5 : A4 : A3 : A2 : A1 : A0 |
+----+----+----+----+----+----+----+----+

 

In Summary:

                       +----+----+----+----+----+----+----+----+
ST HAL requires: | A6 : A5 : A4 : A3 : A2 : A1 : A0 : 0 |
+----+----+----+----+----+----+----+----+

+----+----+----+----+----+----+----+----+
Arduino Wire requires: | 0 | A6 : A5 : A4 : A3 : A2 : A1 : A0 |
+----+----+----+----+----+----+----+----+

 

#I2CAddress #I2CAddressConfusion

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

 

There are many uC companies out there in the world. So obviously me saying "all" was meant as the uC companies that i've used. 

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.