2024-03-20 03:56 AM
Hi there,
after updating to STM32CubeIDE 1.15.0 with H7 Package 1.11.1 H7 ADC3 does no longer offer selection for Temperature Reference, VBat and Vrefint Channels. Screenshot was made with V1.14, missing selections are marked : - ]
Best regards, kdh
Solved! Go to Solution.
2024-04-06 10:08 AM
2024-04-21 10:06 PM
I am running at STM32H747 with the exact same issue. Has anyone got a work-around until there is an official ST update to re-instate these settings?
Thanks
2024-05-01 09:15 AM - edited 2024-05-01 11:05 AM
Hello All,
This issue is fixed in the latest patch release of STM32CubeMX v6.11.1.
Thank you for your contribution and for your patience while we worked on this.
2024-05-06 01:00 PM
Hi Imen,
I have seen, that the new version 1.15.1 offers the ADC3 selection for temperature, vref an vbat again.
Thanks for the repair.
But I have to mention that I had to reinstall the offline repository for the H7. Without this installation, my CubeIDE crashed completely and I had to restart the whole PC.
Best regards
Jens
2024-05-21 05:32 AM
1.15.1 get me further than 1.15.0, but i am now encountering the problem reported here:
2024-05-21 05:35 AM
@rogopodx please follow the thread you provided for updates.