cancel
Showing results for 
Search instead for 
Did you mean: 

Does STM32Cube IDE require internet to operate?

RNK59
Associate II

Once the IDE is installed, is connection to the internet required while using it ?

 

Thanks

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Guru

No, you don't need the internet to build or run projects.

You do need the internet to download firmware packages.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

6 REPLIES 6

It depends what version you have!

I think it was 1.15.x which introduced the requirement to login?

That's why I've stuck with 1.13.0!

 

Also depends on what you mean by "operate"; eg, when starting a new project, it might need to download a new firmware pack - but once that's done, it's done.

Thank you for the reply.

Latest version 1.16 is the one I am referring to.

By operate I mean to build and run projects

 

TDK
Guru

No, you don't need the internet to build or run projects.

You do need the internet to download firmware packages.

If you feel a post has answered your question, please click "Accept as Solution".
RNK59
Associate II

Perfect, thank you!

BarryWhit
Lead II

You do need the internet to download firmware packages.

But it's possible to download them manually from the ST website as zip files(requires account ,grrrr) and then install them offline on another machine (via Help/Manage Embedded Software Packages/From Local). 

- If someone's post helped resolve your issue, please thank them by clicking "Accept as Solution".
- Please post an update with details once you've solved your issue. Your experience may help others.
RNK59
Associate II

Thank you Barry. So essentially, one can download everything needed and then once installed one can go off-line. Great stuff!