2024-05-24 03:39 AM
When working in remote connections, such as WSL or docker the STM32 extension can not be activated with the following error:
"Cannot activate the 'STM32 VS Code Extension' extension because it depends on the 'C/C++ Extension Pack' extension, which is not loaded. Would you like to reload the window to load the extension?"
But the C/C++ extension is loaded and working.
Is there any Work Around available?
2024-06-06 01:26 AM
hi @MAdle.1
we are already checking this issue