STM32 MPUs Software development tools

Ask questions and find answers on STM32 microprocessors software development tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 445 Views
  • 0 replies
  • 0 kudos

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 327 Views
  • 0 replies
  • 0 kudos

STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! System reset during kernel debug

Using MP135F-DK board.Setup the environment and rebuild kernel.After I use openocd and gdb success connect to linux system, try to debug linux kernel, then run some simple gdb command like "bt" or do nothing, then system get reset.I did not get much ...

mingming by Associate II
  • 10625 Views
  • 16 replies
  • 0 kudos

STM32MP135F-DK

Experiencing a 'Connection timed out' error (Failed to execute MI command) in STM32Cube IDE when launching. Looking for assistance with debugger configuration and troubleshooting steps. Any advice appreciated. Thanks!

Screenshot 2023-11-08 104549.png

STM32CubeIDE 1.14.0 released

STM32CubeIDE 1.14.0 was released today on st.com as well as an in-tool update patch. What is new in 1.14.0? Added the support for new microcontrollers in the STM32WB seriesAdded the support for two new boards related to the STM32WB series: NUCLEO-WBA...

STM32CubeProgrammer 2.15.0 released

STM32CubeProgrammer v2.15.0 release informationNew features:• Added the NOR flash memory and OTP fuse programming via USB and UART using OpenBootloader for the STM32MP13xx microprocessors• Added the support for the PMIC programming via UART for the S...

STM32MP1 identify CM4/CA7 assigned periperhals

Hello,with CubeMx 6.9.2 i am generating Code for CubeIDE with the goal to figure out which periphery is assigned to the CA7 or the CM4.With Freemarker it is possible to get information about which IP's are assigned and used but i have no idea how to ...

Jagr by Associate II
  • 1646 Views
  • 0 replies
  • 0 kudos