Skip to main content
GHers.1
Associate
January 2, 2023
Solved

STLINK-V3SET connection to STM32MP157C using CubeProgrammer

  • January 2, 2023
  • 1 reply
  • 1774 views

hello,

I am connecting the STM32MP157C to the debugger using STDC14 CN1 connector in JTAG mode.

Please tell me the pin/signal direction, with regard to the debugger, for the following:

Pin 4, T_JTMS

Pin 6, T_JCLK

Pin 8, T_JTDO

Pin 10, T_JTDI

 

The connection fails using the CubeProgrammer.

I get the following message: "ST-LINK error (DEV_UNKNOWN_MCU_TARGET)".

On the debugger the PWR led lights green and the COM led lights red.

The signals I am using to connect are: T_JTMS, T_JTCK, T_JTDI, T_JTDO (STM32MP157C to debugger) and also providing 3.3V to pin 3, T_VCC and of-course connecting the GND pins.

I am not connecting STM32MP NJTRST pin to pin 12, T_NRST in the debugger (the STM32MP has an internal PU on it).

The STM32MP157C boot mode is JTAG (although doesn't work in USB boot mode).

 

What am I missing here?

 

thanks

Gil

This topic has been closed for replies.
Best answer by PatrickF

Hi @GHers.1​ 

With ST32MPx products (MPUs), the JTAG is only used for debugging, so cannot connect to CubeProgrammer. CubeProgrammer connect using USB.

Debugging with JTAG is using CubeIDE.

See https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Let%27s_start

Regards,

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

1 reply

PatrickF
PatrickFBest answer
ST Employee
January 17, 2023

Hi @GHers.1​ 

With ST32MPx products (MPUs), the JTAG is only used for debugging, so cannot connect to CubeProgrammer. CubeProgrammer connect using USB.

Debugging with JTAG is using CubeIDE.

See https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Let%27s_start

Regards,

In order to give better visibility on the answered topics, please click on 'Select as Best' on the reply which solved your issue or answered your question. See also 'Best Answers'

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent