STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32MP157F GRUB boot command line

I would like to only use cgroup v2 and would like to modify the kernel cmdline boot arguments as follows:, .  I searched internet and suggestion is to useadd systemd. unified_cgroup_hierarchy=1 under /etc/default/grub , followed by sudo update-grub ....

pme991 by Associate II
  • 573 Views
  • 1 replies
  • 0 kudos

Resolved! Boot on STM32MP1

Hello,We're trying to boot our prototype which contains an STM32MP157FAA.Unfortunately, we didn't implement an oscillator/quartz on the board, so we are unable to use HSE and can only use HSI.We have access to USB1, USB2, SDMMC3, and UART4.Is there a...