STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32mp15x emmc reboot stuck-up

Hi,I have a problem with hanging up my board occasionally when an issue from the console reboot.I read about and the internet says this is a problem with the EMMC memory's power cycle.So I followed by a linkhttps://github.com/orangepi-xunlong/openwrt...

MWoło.2 by Senior III
  • 1499 Views
  • 2 replies
  • 0 kudos

Resolved! STM32MP151 emmc OTP configure

Hello. We already have a custom board based on STM32MP151CAD3 with an eMMC. The following pins are different with default eMMC pins.SDMMC2_CMD: PA0SDMMC2_D1: PB7 As not default pins are used, we need to update OTP value. Here are my result. OTP3 = 0x...

Kernel panic after flashing

Hello, I built an image with the following configuration by using the ST wiki pages:STM32MP157D-DK1 Evaluation BoardYocto KirkstoneSTM32MP1-Ecosystem-v4.1.0meta-java layer (branch kirkstone)I have used the following command to create an image:./creat...

enienws by Associate
  • 1087 Views
  • 0 replies
  • 0 kudos

Resolved! STM32MP133 OTP Alternate QSPI Boot

Hello, In order to use the non-default QSPI boot locations, my understanding is port0-port3, 4 signals need to be defined in OTP words 3, 5, and 6 based on a similar question about SDMMC1 discussed here:https://community.st.com/t5/stm32-mpu-products/...

Jasper by Associate II
  • 2803 Views
  • 4 replies
  • 0 kudos