STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FWU Metadata partition protection

Hi,I'm looking at the wic file for STM32MP13 and see two metadata partitions for ATF firmware update. I'm wondering how are these partitions secured from access / modifications from non-trusted world? Since write (and optionally read) operation shoul...

pp2 by Associate II
  • 2551 Views
  • 3 replies
  • 0 kudos

Resolved! How to enable PWM pin

i am facing the issue like i could  not able to access the PWM pinsi want like this only (/sys/class/pwm/pwmchipX/).but i get output like this only. {root@stm32mp1:~# cd /sys/class/pwm/root@stm32mp1:/sys/class/pwm# lsroot@stm32mp1:/sys/class/pwm# ls}...

Resolved! Specific U-BOOT on STM32MP157-D

Hello,I am currently using the STM32MP157D to develop some tests. It seems that a specific U-BOOT has been developed by ST and flashed in the default factory eMMC.On this specific U-BOOT, some self-test commands are interesting.Could it be possible t...

MJ_TS by Associate
  • 1880 Views
  • 1 replies
  • 0 kudos

STM32MP157F GRUB boot command line

I would like to only use cgroup v2 and would like to modify the kernel cmdline boot arguments as follows:, .  I searched internet and suggestion is to useadd systemd. unified_cgroup_hierarchy=1 under /etc/default/grub , followed by sudo update-grub ....

pme991 by Associate II
  • 1582 Views
  • 1 replies
  • 0 kudos