Write image into eMMC when not ST-Link is available on-board?
question no longer required
Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.
question no longer required
Hi everyone. I'm tasked with porting ST's most recent TF-A, u-boot and kernel to a custom stm32mp151c-based board. It runs 2021 version of the above SW components just fine.It seems, however, that at some point the device-tree bindings changed and ...
I built an st-image-weston by using yocto recipes. The layers is in oe-manifest branch scagraph (https://github.com/STMicroelectronics/oe-manifest) I got those warning, please help to fix it. WARNING: st-image-weston-1.0-r0 do_create_flashlayout_co...
hi there I have a question about Memory 。Are the memory regions starting at 0x10000000 and 0x30000000 part of the same mapped area?Are these addresses written the same way in the device tree, or is there a difference between them?thanks,csm
Hi,just a quick question to understand the hardware of the STM32MP257 development kit board: there are several ESD-protection components of type HSP051-4M10 used.What is the exact purpose of them, are they therea) because the DK-board is intended to ...
Hi, I am working with an STM32MP157CAA Rev.Z on a custom STM32CubeMX board running OpenSTLinux 6.6 (Yocto Scarthgap MPU v24.11.06). I have successfully integrated and bootstrapped various boot components.I first got the TF-A and OPTEE to boot the sys...
Hi all,I am trying to get 8th programming language fully working on OpenSTLinux. Currently, it almost fully works, including KMSDRM and Wayland backend suppport using SDL3 for Nuklear based GUI.There seems to be some problem using FFI and libc. "libc...
Hi,on the STM32MP257-DK board, the wires between the MPU and the RAM have an interesting shape:What is the reason for these non-direct wires? Have the same length for all the wires? Shielding? Some noise-thingy?Thanks!
Hallo,I have bought STM32MP135F-DK - Discovery kit and I was working with it few days. I don't know what happened, but today the kit will not work properly - I think the image on SD card is corrupted, some files might by changed or deleted, so I see ...
I have made a custom board with stm32mp135f and now trying to build linux for the custom board.I followed https://wiki.st.com/stm32mpu/wiki/How_to_create_your_own_machineand then run:bitbake core-image-minimaland after 98% got the following error:""E...