cancel
Showing results for 
Search instead for 
Did you mean: 

Wiring between STM32MP257 and RAM?

HMüll.4
Senior

Hi,

on the STM32MP257-DK board, the wires between the MPU and the RAM have an interesting shape:

mp257_dram.png

What is the reason for these non-direct wires? Have the same length for all the wires? Shielding? Some noise-thingy?

Thanks!

 

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

You are working with an LPDDR4 MT53E1G32D2FW-046 on the STM32MP257-DK, which can operate at 2133MHz. At these frequencies, special precautions are necessary to avoid interference and, above all, delayed signals. The last point is achieved by carefully aligning the track lengths, which is noticeable in such zigzag tracks.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

You are working with an LPDDR4 MT53E1G32D2FW-046 on the STM32MP257-DK, which can operate at 2133MHz. At these frequencies, special precautions are necessary to avoid interference and, above all, delayed signals. The last point is achieved by carefully aligning the track lengths, which is noticeable in such zigzag tracks.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.