STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Android support

Hello,Could you explain the reason why Android is not supported on the STM32MP157C-DK2?I can't find any instructions how to install an Android image on the target? The following example references the coprocessor example for A7 and M4 cores, but miss...

Resolved! STM32MP153a failed to boot from eMMC.

Hi there, I am working with a customized STM32MP153A board and trying to boot from eMMC.​I had prepared my eMMC following the steps that I found in <u-boot-stm32mp-2018.11-r0 source code directory>/board/st/stm32mp1/README file:​8. Prepare eMMC======...

BryanWang by Associate II
  • 6392 Views
  • 8 replies
  • 0 kudos

Resolved! STPMIC1 - PONKEYn POWER_ON POWER_DOWN trigger

For STPMIC1, when it is powered on by asserting the PONKEYn signal low, what would happen if the PONKEYn remains asserted low even after the initial POWER_ON trigger? Would it subsequently trigger a POWER_DOWN if PONKEYn long press turn off is activa...

SYEH by Associate II
  • 2518 Views
  • 4 replies
  • 0 kudos

U-boot failed during SD access

Hello CommunityI'm trying to bring up a new architecture board based over STM32MP151aaa core.From what I see from the serial the u-boot prompts leaving the following trace:NOTICE: CPU: STM32MP151AAA Rev.BNOTICE: Model: STMicroelectronics custom STM32...

Resolved! Power Supply for STM32MP157C-DK2

Hello,We would like to setup the STM32MP157C-DK2 board. But we couldn't find any information related to the recommended power supply. Could you please suggest us that which Power Supply 5V/3A adapter or connector should we use? It would be great if y...