STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using RAUC with openstlinux

We are using rauc to perform remote updates on your target devices.However, to create the rauc bundle, rauc uses a different image format than the ST image created.The default imagesource in rauc is:imgsource = "%s-%s.%s" % (d.getVar('RAUC_SLOT_%s' %...

meiss.M by Associate III
  • 4610 Views
  • 7 replies
  • 0 kudos

Resolved! STPMIC1 on I2C2 breaks ATF? Bug?

I'm currently working with the Seed STM32MP1 SoM which has STPMIC1 attached to I2C2. I've been working on setting up a device tree for it, but I've been hitting some bugs. When booting the mainline ATF with my device tree (modified DK2 board, just wi...

JGuy1 by Associate II
  • 2047 Views
  • 1 replies
  • 0 kudos

STM32mp1 perf counters issue ?

Hi,I'm trying to have some accurate perf measurements with the STM32MP1 for my program on Linux. I've tried several things, among them to use perf Linux tool.The number of cycles does not match the time elapsed, i.e. the freq processor is at 650Mhz a...

Kurt by Associate
  • 1218 Views
  • 1 replies
  • 0 kudos

Resolved! ST Link port on DK2 board not working

I'm trying to connect to my DK2 from STM32CubeIDE but the ST LInk port doesn't seem to work. In Device Manager I see "Unknown USB Device (Device Descriptor Request Failed)". I tried several cables and ports on my PC.I should mention that I'm running ...