2020-07-09 2:44 AM
We are using rauc to perform remote updates on your target devices.
However, to create the rauc bundle, rauc uses a different image format than the ST image created.
The default imagesource in rauc is:
imgsource = "%s-%s.%s" % (d.getVar('RAUC_SLOT_%s' % slot), machine, img_fstype)which I edited to:
imgsource = "%s-%s-%s.%s" % (d.getVar('RAUC_SLOT_%s' % slot), "openstlinux", machine, img_fstype)What would be the best way to comply with the filenames created by the ST yocto distribution?
What do you suggest?
2020-07-09 2:54 AM
Hello @meiss.M ,
The issue comes from stm32 extension files which are not supported by RAUC.
I would recommand to apply the following patch in RAUC :
diff --git a/src/update_handler.c b/src/update_handler.c
index bcd6fd8..c77d7f8 100644
--- a/src/update_handler.c
+++ b/src/update_handler.c
@@ -1520,6 +1520,7 @@ typedef struct {
RaucUpdatePair updatepairs[] = {
{"*.ext4.caibx", "ext4", img_to_fs_handler},
{"*.ext4.caibx", "raw", img_to_raw_handler},
+ {"*.stm32", "raw", img_to_raw_handler},
{"*.vfat.caibx", "raw", img_to_raw_handler},
{"*.ubifs.caibx", "ubivol", img_to_ubivol_handler},
{"*.ubifs.caibx", "ubifs", img_to_ubifs_handler},BR,
Christophe
2020-07-09 3:06 AM
Thanks for this, I will try.
Do you recommend using a custom uboot.env script and a copy of the root device?
by adding in st-machine-common-stm32mp.inc :
PARTITIONS_CONFIG[rootfsrauc] ?= "${IMAGE_BASENAME},rootfs,,${ROOTFS_PARTITION_SIZE},FileSystem"
(after PARTITIONS_CONFIG[rootfs] ?= "${IMAGE_BASENAME},rootfs,,${ROOTFS_PARTITION_SIZE},FileSystem")
BTF, this is much more convenient in dunfell now.
Greetings, Markus
2020-07-09 5:26 AM
Hi @meiss.M ,
I'am not sure to catch what you want to do : could you please elaborate for which purpose you need to use a custom u-boot env script ?
BTY, you will have to add u-boot-fw-config-stm32mp recipe to you image to allow RAUC to read and write into u-boot env.
BR,
Christophe
2020-07-09 5:39 AM
We have built up RAUC with symmetric ROOTFS slots: https://rauc.readthedocs.io/en/latest/scenarios.html#symmetric-root-fs-slots
> BTY, you will have to add u-boot-fw-config-stm32mp recipe to you image to allow RAUC to read and write into u-boot env.
Yes i did this - it works, by patching the thud uboot for adding the respective stm32mp15_trusted_defconfig
Luckily in dunfell it is included, which makes it possible to update the uboot fw env
is this the recommended way to add the additional rootfs :
> PARTITIONS_CONFIG[rootfsrauc] ?= "${IMAGE_BASENAME},rootfs,,${ROOTFS_PARTITION_SIZE},FileSystem"
2020-07-09 8:37 AM
Hi @meiss.M ,
There is no specific recommended way to add the additional rootfs on STM32MP1.
Nevertheless, a proposition would to build a rootfs image for A, flash this image for both A and B, but you need to run post-install.sh script after flashing B to update partition mount points (kernel cmdline, vendorfs ....). Hope I'am clear enough.
BR,
Christophe
2020-07-29 3:16 AM
Hello @Christophe Guibout ,
Thank you for your advice,
can you please post me your system.conf
mine looks like this:
# rauc configuration file
[system]
compatible=SDM array
bootloader=uboot
statusfile=/boot/raucstatus
[autoinstall]
path=/data/fw_update
[keyring]
path=/etc/rauc/ca.cert.pem
# [handlers]
# post-install=/sbin/resize-helper # from thud
# [slot.bootfs.0]
# device=/dev/mmcblk0p4
# type=ext4
[slot.rootfs.0]
device=/dev/mmcblk0p6
type=ext4
bootname=system0
[slot.rootfs.1]
device=/dev/mmcblk0p7
type=ext4
bootname=system1device=/dev/mmcblk0p7 is the added root device (slot B)
2020-07-29 3:56 AM
Hello @meiss.M ,
Here is mine :
[system]
compatible=stm32mp1
bootloader=uboot
mountprefix=/mnt/rauc
max-bundle-download-size=805306368
[keyring]
path=/etc/rauc/ca.cert.pem
[handlers]
post-install=/usr/lib/rauc/post-install.sh
[slot.rootfs.0]
device=/dev/mmcblk1p13
type=ext4
bootname=A
[slot.rootfs.1]
device=/dev/mmcblk1p14
type=ext4
bootname=B
[slot.bootfs.0]
device=/dev/mmcblk1p9
type=ext4
parent=rootfs.0
[slot.bootfs.1]
device=/dev/mmcblk1p10
type=ext4
parent=rootfs.1
[slot.vendorfs.0]
device=/dev/mmcblk1p11
type=ext4
parent=bootfs.0
[slot.vendorfs.1]
device=/dev/mmcblk1p12
type=ext4
parent=bootfs.1BR,
Christophe