STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! MP1 SPINAND boot needs HSE ?

We use HSE osc instead of xtal as suggested by errata. However to support STANDBY we need to turn it off by GPIO. The idea is to boot from SPINAND on HSI and turn HSE in bootloader.Unfortunately it seems that ROM hangs when HSE is not present:< @ 006...

GUI doesnt loads post ST Banner after USART changes in STM32MP157C-DK2 board. DIsplay controller probe failure -22

Hello, I have done the modification in the device tree related to inclusion of usart3 as per 3.3.1 Activation of a USART or UART instance in https://wiki.st.com/stm32mpu/wiki/Serial_TTY_device_tree_configuration&usart3 { pinctrl-names = "default", "s...

darla14 by Senior
  • 1707 Views
  • 1 replies
  • 0 kudos

Wakeup on GPIO in Linux on STM32MP1

Hello. I am working on standby/wakeup using gpio pin in stm32mp1 custom board. Going to sleep works well using gpio-keys but I can't wakeup. What bothers me most is that interrupt responsible for waking up does not set "waleup" attribute although it ...

RPiet.1 by Associate II
  • 7386 Views
  • 11 replies
  • 1 kudos

WEBINAR: Register today to learn how performance analysis assists with developing extraordinary experiences on the STM32MP1

Whether it's to minimize computational power, improve the device's output or keep the GUI from freezing or crashing, debugging embedded software can be a challenging and time-consuming step in the process of developing embedded devices.With a multitu...

SSnid.1 by Associate II
  • 1009 Views
  • 0 replies
  • 0 kudos