STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

WpeWebkit GPU performance issues

Hello,we have product based on a STM32MP157 running Linux. The distribution is based on Yocto kirkstone and we are using a 6.1.82 Kernel. For the MP1s' GPU we use the open source entaviv driver that ships with this kernel. The device has a graphical ...

hmmtr by Associate
  • 2768 Views
  • 4 replies
  • 1 kudos

STM32MP257FAI3 – Some GPIO pins (e.g., PZ7, PZ8) still consumed by kernel even after removing from pinctrl in TF-A, U-Boot, and Linux

 Hello ST Community,I am currently working on a custom board based on STM32MP257FAI3, derived from the STM32MP257F-EV1 evaluation board.We initially built our own custom image and successfully enabled several peripherals (SPI, USART, Timers, ADCs, an...

_Krishna by Associate III
  • 658 Views
  • 3 replies
  • 0 kudos

Resolved! Failing ETH2 on STM32MP2

Hi, I have a custom board based on STM32MP257FAK3, based on STM32MP257EV1 evaluation board. My board has a rtl8367s ethernet switch connected on eth2 port though rgmii. I can communicate though mdio to the rtl8367s and configure it. We are using Open...

jcalvo by Associate II
  • 1816 Views
  • 9 replies
  • 0 kudos