STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Inaccurate measurement of VREFINT

Hi everyone!I see unexpected values when measuring VREFINT. The ADC measures around 1.18V, on some boards even 1.16V, which is outside the tolerance according to the datasheet: Reading the calibration value VREFIN_CAL from OTP memory returns a value ...

0693W00000QLsweQAD.png 0693W00000QLsozQAD.png
jvog.sen by Associate II
  • 5622 Views
  • 7 replies
  • 0 kudos

gdbgui and STLink debug

From instructions, I opened two console: Console 1: openocd -f board/stm32mp15x_dk2.cfg This looks good as output:   ``` ... Info : stm32mp15x.cm4: Cortex-M4 r0p1 processor detected Info : stm32mp15x.cm4: target has 6 breakpoints, 4 watchpoints Info ...

Dat Tran by Senior II
  • 2817 Views
  • 2 replies
  • 0 kudos

Resolved! How to hide OTP values on STM32MP15

From user manual, from OTP word 59th for user to store sensitive information, meaning there is a way to prevent read them by STM32cube tool for non-secure application.We see the way to lock them which mean can't not change values, any document that t...

Dat Tran by Senior II
  • 2679 Views
  • 5 replies
  • 0 kudos

Resolved! stm32mp157c implementation initramfs

Hi,I usestm32mp157c and the filesystem runs emmc default. But I want it to change it and run at ramfs. I addedCONFIG_BLK_DEV_INITRD=yCONFIG_RD_GZIP=yCONFIG_RD_BZIP2=yCONFIG_RD_LZMA=yCONFIG_RD_XZ=yCONFIG_RD_LZO=yCONFIG_RD_LZ4=yin kernel config file. A...

aliMesut by Associate III
  • 2435 Views
  • 1 replies
  • 0 kudos

Resolved! STM32MP151 - How to activate MCO ?

Hello, I'm trying to leverage the MCO capability of the STM32MP1, but I don't success. I want to have LSE on MCO1 and HSE on MCO2. I'm using TFA -> uboot -> linux and I can build with Yocto or Buildroot.Which steps should be done during TFA, uboot an...