STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! libqmi build for STM32MP157

I'm building libqmi for the STM32MP157 and getting an error  at this point in the build GISCAN Qmi-1.0.girTraceback (most recent call last):File "/home/ed/STM32MPU_workspace/STM32MP1-Ecosystem-v4.1.0/Developer-Package/SDK/sysroots/cortexa7t2hf-neon-v...

edwardmcl by Associate II
  • 2821 Views
  • 2 replies
  • 0 kudos

STM32MP1 boot fail in TF-A

Hi all,We design the custom board use ST32MP157 base on the design of STM32MP157-DK2 kit. We use the SD card for booting. The image and device tree is custom base on example of STM32MP157-DK2 kit. The board has a issue when booting via SD card. This ...

Resolved! stm32mp135f trusted vs optee efficiency

Hello, For some time I testing STM32MP135f with 1GHz CPU clocking. I was able to generate optee OpenStLinux but I see a lack of CPU efficiency. I'm curious what is the difference in efficiency between trust and optee. If I use the trusted option the ...

MWoło.2 by Senior III
  • 2197 Views
  • 2 replies
  • 1 kudos

OpenAmp_TTY_echo not creating rpmsg0|1

Hello,Searched around but couldn't find a similar issue.Please point me to one if one exist. I have a custom board with the stm32mp157c mounted. Board works fine, trying to communication between the m4 and a7 processor using the rpmsg devices. I have...

mantwih by Associate III
  • 1942 Views
  • 1 replies
  • 0 kudos