STM32WLEx: Generated Binary file size is too large
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-04 2:01 AM
Before release of package v1.3.0 binary size were <90kb and .ld has 3 partition in memory as below,
/* Memories definition */
MEMORY
{
ROM (rx) : ORIGIN = 0x08000000, LENGTH = 256K
RAM1 (xrw) : ORIGIN = 0x20000000, LENGTH = 32K /* Non-backup SRAM1 */
RAM2 (xrw) : ORIGIN = 0x20008000, LENGTH = 32K /* Backup SRAM2 */
}
But release package v1.3.0 has generated large binary size 250KB for Release and Debug build of LoRaWAN example. In this release ST has introduced the changes in .ld file as below,
/* Memories definition */
MEMORY
{
RAM1 (xrw) : ORIGIN = 0x20000000, LENGTH = 32K
NVM_RAM (rw) : ORIGIN = 0x20008000, LENGTH = 4K
RAM2 (xrw) : ORIGIN = 0x20009000, LENGTH = 28K
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 248K
USER_Key_region_ROM (rx) : ORIGIN = 0x0803E500, LENGTH = 768
}
Here, USER_Key_region_ROM (rx) partition is newly introduced and due to this change binary size is become way to large.
Link for v1.3.0 https://www.st.com/en/embedded-software/stm32cubewl.html
Can you please suggest me how can i reduce the binary file size in the release v1.3.0?
Attaching .ld file of release v1.3.0 for more details
- Labels:
-
Flash
-
STM32WL series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-05 6:10 AM
Made changes in .ld file to reduce the size of the binary. Created USER_FLASH partition with szie of 1kb between FLASH and USER_Key_region_ROM and used fill() command to initialize memory of USER_FLASH partition.
In this case binary size is fixed to the length(around 118K) of FLASH partition but it is working. Not sure this is an appropriate solution or not. also with this solution binary size will always fixed to the LENGTH of FLASH
Attaching modified .ld file
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-05 6:28 AM
The problem with a binary image is that it must be a singular contiguous blob.
If you've created holes / voids you should perhaps be using a .HEX or object file format.
Some tools can decompose a multi-section object into multiple .BIN files.
At the moment you have one .BIN describing memory from 0x08000000 thru at least 0x0803E500, so 249KB+
Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-04-28 12:58 AM
I do not undestand the new memory definition...
What is NVM_RAM (rw)??
From my point of view, i undestand that this FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 248K means that you have 248K for your binary from 0x08000000 thru at least 0x0803E500 (0x08000000- 0x0803E500= 0x3E500 in decimal 248K).
Then, you have from 0x0803E500 to 0x0803E800 USER_Key_region_ROM (rx). 768 bytes.
But you have 248KB + 768 Bytes assignned, and FLASH memory have 256KB of capacity. You have more than 7KB unsigned...
In the code in Lorawan_end_node i can see that use the last two pages of FLASH to store Lorawan context info( in LORAWAN_NVM_BASE_ADDRESS ((void *)0x0803F000UL). Save data structure 1484 bytes in pre-allocated ROM page of 2 Kbytes.
Why FLASH only have 248KB? Would be needed to add another section called FLASH_USER or similar with the rest 7KB of FLASH unassigned?