2023-04-28 12:26 AM
Hello,
I am developing my own project based on Lorawan_end_node project, i have some doubts regarding to memory addressing.
In linker file:
/* Memories definition */
MEMORY
{
RAM1 (xrw) : ORIGIN = 0x20000000, LENGTH = 32K
NVM_RAM (rw) : ORIGIN = 0x20008000, LENGTH = 4K
RAM2 (xrw) : ORIGIN = 0x20009000, LENGTH = 28K
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 248K
USER_Key_region_ROM (rx) : ORIGIN = 0x0803E500, LENGTH = 768
}I don not unsdestand NVM_RAM section, what is it? and USER_Key_region_ROM?
I am trying to optimizate LoRaWAN NVM Context save proccess in FLASH. By default it is saved in
#define LORAWAN_NVM_BASE_ADDRESS ((void *)0x0803F000UL)
It would be the last two pages(2x2kB) of flash memory in case FLASH memory LENGTH would be 256K as expected..
Normally, another section would be present, something like this
USER_FLASH (rx) : ORIGIN = 0x0803F000UL , LENGTH = 4K
Can someone help me to undestand this?
Regards,
2023-04-28 8:32 AM
Hello @RPaja.1 and welcome to ST Community.
I advise you to check these resources :
hope this is helpful
Issam
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.