I'm using Bluenrg-M2SA with and facing issue with ble connection. Bluenrg-M2SA is connecting as a client with smart watch but it gets disconnected at every 30 seconds. Error: hci_disconnection_complete_event, Reason: 13I'm using BlueNRG-1_2 DK 3.2...
Hello, we are working on new release of STM32WL "STM32Cube_FW_WL_V1.3.0". release which has introduced changes in RTC driver which we believe is fixed for the issue (RTC loosing time issue STMicroelectronics/STM32CubeH7#24 )But, after running RTC ove...
I'm using Bluenrg-M2SA with and facing same with ble connection. Bluenrg-M2SA is connecting with smart watch but GATT procedure issues a timeout at 30 seconds. using BlueNRG-1_2 DK 3.2.3. Any idea to increase the connection time from application?
Made changes in .ld file to reduce the size of the binary. Created USER_FLASH partition with szie of 1kb between FLASH and USER_Key_region_ROM and used fill() command to initialize memory of USER_FLASH partition.In this case binary size is fixed to t...
we have made changes in capacitance and now with release v1.3.0 module is providing correct time.we have tested continuously 4 days and haven't seen any missing seconds on logs. thank you guys for the suggestion and quick support
Hi @MAndreka Set TXParams(...) command is used to set the TX output power of Lora radio SX1261/62. All SubGhz commands details are available in semtech datasheet which you can download from https://www.semtech.com/products/wireless-rf/lora-connect/s...