2019-05-27 4:06 AM
Hello everyone,
Due to an increasing number of people having issues with CubeIDE and TouchGFX Integration i'm attaching a working project for STM32F746G-DISCO for your inspection - There were a good number of things to do before it worked, only some of which i highlighted in my quick-guide and even some of those steps were a bit ambiguous and could be executed in different ways.
I've written down what i've done to get this project working and i will use this in planning a video tutorial - It has to be somewhat official, so i can't simply start up the screencast and start talking. But i'll keep you updated.
/Martin
2019-11-21 1:58 AM
I have solved this first problem adding these lines
int main(void)
{
/* USER CODE BEGIN 1 */
DBGMCU->APB1FZ = 0xFFFFFFFF;
DBGMCU->APB2FZ = 0xFFFFFFFF;
/* USER CODE END 1 */
2019-11-21 2:00 AM
but now the interface run but I cannot arrive to my while(1) because the code go in loop inside the function osKernelStart();
/* Start scheduler */
osKernelStart();
/* We should never get here as control is now taken by the scheduler */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
GPIO_InitTypeDef GPIO_InitStructure;
GPIO_InitStructure.Pin = GPIO_PIN_1;
GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStructure.Pull = GPIO_NOPULL;
GPIO_InitStructure.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOI, &GPIO_InitStructure);
while (1)
{
/* USER CODE END WHILE */
//HAL_GPIO_TogglePin(Ld1_GPIO_Port, GPIO_PIN_1); //Toggle LED
if (HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_1)) {
HAL_GPIO_WritePin(GPIOI, GPIO_PIN_1, GPIO_PIN_RESET);
} else {
HAL_GPIO_WritePin(GPIOI, GPIO_PIN_1, GPIO_PIN_SET);
}
HAL_Delay(5000); //Delay 1 Seconds
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
2020-04-11 2:07 AM
hi. When i open file of touchGFX from STM32cubeIDE, i have massage: touchGFX contains spaces, this can result in erroneous behaviour while compiling. So, i can't generate code my application. Please help me, solve it. thanks
2020-04-13 11:53 AM
This thread is very old. Are you actually using CubeIDE 1.0.0 and TouchGFX 4.13.0?
You should really update to the latest version. The follow thread is about the new versions:
https://community.st.com/s/question/0D50X0000BwjU6pSQE/official-release-xcubetouchgfx-v4130
2020-10-29 12:13 AM
hello friend
Touchgfx does not work for me, I get the pixelated screen I use stm32cubeide 1.4.0 it does not work for me download version 1.2.0 and also download TouchGFX V4.14 and nothing, change the version ==> V4.13 and still some help friend , I hope you can help me ??
I made a simple program in touchgfx and there it works, but the detail is that I use LWIP in my program, I need to use it from stm32cubeide
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.