2022-11-11 11:17 AM
Hello,
A hard fault exception is being thrown when I flash the SBSFU_userapp.bin file with the STM32Cube Programmer to device that uses the WB55 MCU architecture (M4/M0+) and then try to run the SBSFU example in Tera Term. The secure engine is first initialized and then hits the hard fault error after "CHECK USER FW STATUS" then loops again to the secure engine initialization and continues this process until I disconnect from the device from Tera Term. I have provided a screenshot to illustrate the issue. I don't have any idea on how to debug this and would appreciate any feedback on this issue and how I can go about resolving it.
Hardware:
Software:
2022-11-14 1:14 AM
Hello @SERT,
the example is supposed to work out of the box.
I would suggest restarting from scratch and follow readme file.
If it does not change anything, only way to understand what happens is to use debugger. For this you will need to deactivate security protections such as RDP, WRP and others.
Best regards
Jocelyn
2022-11-24 5:54 AM
Hi @SERT,
what's the FW on the M0 part? Is it active? You can use the CubeProgrammer to check.
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.