User Activity

Hello,The new SBSFU 2.6.1 is available now.The main change concerns the compatibility with latest STM32CubeIDE based on GNU Tools 10.3 which are version 1.9.0 and 1.10.1There is no need anymore to follow the steps provided previously to have a succes...
Hello SBSFU users !The latest release of STM32CubeIDE 1.9.0 is introducing GNU Tools version 10.3 as toolchain. This new toolchain creates an issue in the SBSFU final build.A new release of X-CUBE-SBSFU is coming in around one month to fix this but, ...
As well as for TFM case, some IT tools remove exe files.The SBSFU is using:c:\STM32SecuWS\L4\STM32CubeExpansion_SBSFU_V2.3.0\Middlewares\ST\STM32_Secure_Engine\Utilities\KeysAndImages\win\prepareimage\prepareimage.exeIf this file was removed, please ...
Sometimes, the windows exe file are not recognized as valid programs by internal IT tools.The TFM uses windows exe file to build the image signature.A way to solve this you need to use python:Install python 3.7Create a requirements.txt file containin...