2024-03-05 02:37 AM - edited 2024-03-05 03:07 AM
Hi all,
I am using STM32F769I DISCO Board, STM32 CUBEIDE,X-CUBE-SBSFU 2.6.2 , WINDOWS Environment for checking new features in security i.e. secure bootloader.
I am newbie to this topic and I have followed compilation procedure as per the readme file, but I am getting file missing error in MDK-ARM IDE
SE_CoreBin.s(19): error: A1270E: File "..\..\1_Image_SECoreBin\MDK-ARM\STM32F769I_Discovery_1_Image_SECoreBin\SECoreBin.bin" not found
and in CUBEIDE :
"../prebuild.sh" "../"
prepareimage with python script
python /prepareimage.py conf ..//../Inc/se_crypto_config.h
python: can't open file 'C:\\prepareimage.py': [Errno 2] No such file or directory
selected
../prebuild.sh: line 54: can't create ..//Application/Startup/se_key.s: nonexistent directory
../prebuild.sh: line 55: can't create ..//Application/Startup/se_key.s: nonexistent directory
../prebuild.sh: line 56: can't create ..//Application/Startup/se_key.s: nonexistent directory
../prebuild.sh: line 135: can't create ..//Application/Startup/se_key.s: nonexistent directory
recopy postbuild.sh script with .sh script
cat: can't open '..//.sh': No such file or directory
cat ..//.sh : failed
make[1]: *** [makefile:94: pre-build] Error 1
make: *** [makefile:62: all] Error 2
"make all" terminated with exit code 2. Build might be incomplete
I tried these steps but it didn't helped me
Note : 1. I tried to give proper python path in system environment variable.
2. I copied Zip file in C drive created one folder unziped.(No space or & in path).
3. delete project from workspace add it again clean it and rebuild.
Solved! Go to Solution.
2024-03-05 04:31 AM
Hello @lavanya ,
Which STM32CubeIDE version and MDK-ARM version are you using?
It is mentioned in the release note projects of X-CUBE-SBSFU Expansion package that the development toolchain and compiler used for this package is STM32CubeIDE v1.9.0 and MDK-ARM V5.31.
For that please try to update the STM32CubeIDE toolchain.
Also, possible build issues may be caused by too long path names. I suggest you to unzip the package in a short path like e.g. C:\work.
May this discussion can help you.
Please let me know if the issue is solved or not.
I hope this help you!
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-03-05 04:31 AM
Hello @lavanya ,
Which STM32CubeIDE version and MDK-ARM version are you using?
It is mentioned in the release note projects of X-CUBE-SBSFU Expansion package that the development toolchain and compiler used for this package is STM32CubeIDE v1.9.0 and MDK-ARM V5.31.
For that please try to update the STM32CubeIDE toolchain.
Also, possible build issues may be caused by too long path names. I suggest you to unzip the package in a short path like e.g. C:\work.
May this discussion can help you.
Please let me know if the issue is solved or not.
I hope this help you!
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.