SBSFU File Missing error bin file of SECoreBin in STM32F769I MCU
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-05 2:37 AM - edited ‎2024-03-05 3:07 AM
Hi all,
I am using STM32F769I DISCO Board, STM32 CUBEIDE,X-CUBE-SBSFU 2.6.2 , WINDOWS Environment for checking new features in security i.e. secure bootloader.
I am newbie to this topic and I have followed compilation procedure as per the readme file, but I am getting file missing error in MDK-ARM IDE
SE_CoreBin.s(19): error: A1270E: File "..\..\1_Image_SECoreBin\MDK-ARM\STM32F769I_Discovery_1_Image_SECoreBin\SECoreBin.bin" not found
and in CUBEIDE :
"../prebuild.sh" "../"
prepareimage with python script
python /prepareimage.py conf ..//../Inc/se_crypto_config.h
python: can't open file 'C:\\prepareimage.py': [Errno 2] No such file or directory
selected
../prebuild.sh: line 54: can't create ..//Application/Startup/se_key.s: nonexistent directory
../prebuild.sh: line 55: can't create ..//Application/Startup/se_key.s: nonexistent directory
../prebuild.sh: line 56: can't create ..//Application/Startup/se_key.s: nonexistent directory
../prebuild.sh: line 135: can't create ..//Application/Startup/se_key.s: nonexistent directory
recopy postbuild.sh script with .sh script
cat: can't open '..//.sh': No such file or directory
cat ..//.sh : failed
make[1]: *** [makefile:94: pre-build] Error 1
make: *** [makefile:62: all] Error 2
"make all" terminated with exit code 2. Build might be incomplete
I tried these steps but it didn't helped me
Note : 1. I tried to give proper python path in system environment variable.
2. I copied Zip file in C drive created one folder unziped.(No space or & in path).
3. delete project from workspace add it again clean it and rebuild.
Solved! Go to Solution.
- Labels:
-
SBSFU
-
STM32 Security
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-05 4:31 AM
Hello @lavanya ,
Which STM32CubeIDE version and MDK-ARM version are you using?
It is mentioned in the release note projects of X-CUBE-SBSFU Expansion package that the development toolchain and compiler used for this package is STM32CubeIDE v1.9.0 and MDK-ARM V5.31.
For that please try to update the STM32CubeIDE toolchain.
Also, possible build issues may be caused by too long path names. I suggest you to unzip the package in a short path like e.g. C:\work.
May this discussion can help you.
Please let me know if the issue is solved or not.
I hope this help you!
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-05 4:31 AM
Hello @lavanya ,
Which STM32CubeIDE version and MDK-ARM version are you using?
It is mentioned in the release note projects of X-CUBE-SBSFU Expansion package that the development toolchain and compiler used for this package is STM32CubeIDE v1.9.0 and MDK-ARM V5.31.
For that please try to update the STM32CubeIDE toolchain.
Also, possible build issues may be caused by too long path names. I suggest you to unzip the package in a short path like e.g. C:\work.
May this discussion can help you.
Please let me know if the issue is solved or not.
I hope this help you!
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.