cancel
Showing results for 
Search instead for 
Did you mean: 

Where can I get latest version CMSIS DSP lib ( .a file) (CMSIS version 5) file for STM32F7

AN.4
Associate II
 
7 REPLIES 7
Mike_ST
ST Employee

Hello,

In the STM32F7 firmware package,

there is a directory where you can find precompiled libs (CMSIS 5.4) :

STM32Cube_FW_F7_V1.16.1\Drivers\CMSIS\Lib

AN.4
Associate II

Hello Mike,

Thanks for the response.

I am looking for CMSIS 5.8.0 which includes DSP v1.9.0.

If CMSIS 5.8.0 version's library files are available, please let me know

Mike_ST
ST Employee

Sorry that it doesn't fit your need.

The latest we are using is CMSIS 5.6.0/DSP 1.7.0 for STM32H7.

Hi Mike,

i want to use the QuaternionMathFunctions of the DSP v1.9.0 on an STM32F446RE.

I downloaded CMSIS 5.8.0 from github but it seems that the directory does not contain the precompiled libraries, nor the c files.

Is DSP v1.9.0 also not available for STM32F4? And is there a way that I could compile the library myself?

I would be very glad to receive an answer.��

Hi,

Did you able to figure out how to use quaternion math functions from DSP library. I downloaded latest CubeMx and the version of the DSP is 1.5.2 as shown below

0693W00000WJlo4QAD.pngIt misses lot of functionalities like matrix vector operations.

Thanks in advance.

Thanks for your pormpt reply.

Just to update you and everyone who come across this discussion, following is the updated link to the CMSIS-DSP

https://arm-software.github.io/CMSIS-DSP/latest/