cancel
Showing results for 
Search instead for 
Did you mean: 

STLINK debugging issue in stop mode (STM32U031C8U6)

GiuseppeB
Associate II

Hi all,

I'm having trouble debugging using STLINK when the STM32U031C8U6 microcontroller is in stop mode or running at a low frequency clock

I already tried to:

  • enable in the STM32CubeIDE the "Debug in low power modes" option (Debug Configuration, Debugger tab)
  • call the HAL_DBGMCU_EnableDBGStopMode() function at the begin of application.

 

Issue #1

Attached is a minimal project that reproduces the problem I'm having using the low-power timer peripheral. I'd like to use it to exit stop mode every 2 ms or every 10 ms based on some conditions, which I've simulated here with the state of a push button.

The project works correctly if I use the STLINK debugger to flash the microcontroller and then disconnect it to run in standalone mode.

However, I experience an unexpected behavior when running it in debug mode with STLINK debugger.

The microcontroller runs at a 16 MHz HSI clock and the LPTIM1 peripheral uses an external 32.768 kHz crystal.

Looking at the main() function, you can see that after initialization, it waits for a button press and then sets the two periods mentioned above in LPTIM1. 

The BSP_LPTIM_Setup() function performs the following operations:

  • Enables the TIMOUT function
  • Enables the LPTIM1 peripheral
  • Enables the Autoreload match interrupt
  • Sets the CCR1 compare period to approximately 2 ms: (2 << 5) / 32768
  • Sets the ARR autoreload period to approximately 10 ms: (10 << 5) / 32768

At this point, we enter the superloop, which simply:

  • Sets the desired period based on the button state. The BSP_LPTIM_SetTimeout() function:
    • Does nothing if the requested period is equal to the current one; otherwise,
    • Enables the Compare match interrupt if the requested period is 2 ms and disables it if it is 10 ms.
  • Start the timer in ONESHOT mode (BSP_LPTIM_Start function()).
  • Enter stop mode.

The interrupt callbacks simply reset the counter and toggle the PROBE pin that I use for testing.

The behavior I get in standalone mode is as expected: depending on the state of the button, the micro is woken up every 2 ms by HAL_LPTIM_CompareMatchCallback() or every 10 ms by HAL_LPTIM_AutoReloadMatchCallback().

Instead, the behavior I see in debug is this:

  • when the button is pressed, the PROBE pin toggles approximately every 4 ms.
  • when the button is released, the PROBE pin never toggles.

 

Issue #2

If in the same project I change the ABH Prescaler from /1 to /256 to reduce the HCLK to 62.5 kHz, I have to reduce the STLINK frequency to 1000 kHz to be able to debug, and that's fine.

At this point I experience another unexpected behavior: the execution of the SystemClock_Config() function seems to be continually interrupted by the SysTick_Handler().

If I add a breakpoint anywhere in the main() function after SystemClock_Config() and start debugging, it never gets reached. 

If I suspend the execution, I see that I'm still inside the SysTick_Handler().

 

Thanks in advance,

G.

1 REPLY 1
Billy OWEN
ST Employee

Hi @GiuseppeB 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy