cancel
Showing results for 
Search instead for 
Did you mean: 

UART Transmitting issue or any other issue

AHayee
Associate II

Hi Everyone,

I am using STM32F407DISCO board and made a simple program which transmit some values. The program is as follows

 

#include "stm32f4xx_hal.h"
#include "main.h"

UART_HandleTypeDef USART2Config;


void GPIO_Init(void);
void UART2_Init(void);
void Err_Handle(void);

char data[] = "Hello";
uint8_t value = 43;
uint16_t value2 = 1024;
char buffer[10];

int main(){

	HAL_Init();
	GPIO_Init();
	UART2_Init();


	HAL_GPIO_WritePin(GPIOD, RED_LED, 1);
	HAL_GPIO_WritePin(GPIOD, GREEN_LED, 1);
	HAL_GPIO_WritePin(GPIOD, ORANGE_LED, 1);
	HAL_GPIO_WritePin(GPIOD, BLUE_LED, 1);

	HAL_UART_Transmit(&USART2Config, (uint8_t*) data, strlen (data), HAL_MAX_DELAY);
	HAL_UART_Transmit(&USART2Config, &value, 1, HAL_MAX_DELAY);
	HAL_UART_Transmit(&USART2Config, (uint8_t*) &value2, sizeof(value2), HAL_MAX_DELAY);

	while(1){

	}
}

 

 

 

 

The code above only Transmit line 28 and 29, Line 30 not transmitted.

but when I comment out Line 28 then line 29 and 30 transmitted.

What I am doing wrong here? 

Following is the logic analyzer waveform when Line no 28,29 and 30 are transmitted.

AHayee_0-1726491245079.png

Following is the logic analyzer waveform when Line no 29 and 30 are transmitted

AHayee_1-1726491391625.png

Kindly correct me where I am making mistake.

Thanks and best regards

1 ACCEPTED SOLUTION

Accepted Solutions
AHayee
Associate II

The issue is resolved after I added the following function

void SysTick_Handler(void){
	HAL_IncTick();
	HAL_SYSTICK_IRQHandler();
}

Thanks everyone for your support 

View solution in original post

8 REPLIES 8

Is there any error or warning during compilation?

JW

If you single-step those lines, does each one transmit?

Do any of the HAL_UART_Transmit() calls return an error?

AHayee
Associate II

@waclawek.jan  No there is no error or warning while compilation

@Andrew Neil No I didn't check the single-step nor I checked if any error is returning.

How do I check if it is returning any error or not?


@AHayee wrote:

How do I check if it is returning any error or not?


The same way you'd check the return value from any function call:

 

HAL_StatusTypeDef result;
:
:
   result = HAL_UART_Transmit( &USART2Config, (uint8_t*) data, strlen (data), HAL_MAX_DELAY );
   if( result != HAL_OK )
   {
      // An error occured!
   }

 

 


@AHayee wrote:

I am using STM32F407DISCO board 


How are you connecting to the UART?

This board requires you to make the connection manually from the UART to the ST-Link's VCP:

AndrewNeil_0-1726499161524.png

Are you sure that your connections are secure & reliable?

Try to transmit something also in the while() loop, e.g. the "Hello" string, in a loop.

JW

Karl Yamashita
Principal

Looks like you're re-inventing the wheel

 

UART_HandleTypeDef USART2Config;

 

Show your configuration.

 

And where is you System Clock configuration? Are you relying on HSI?

What is APB1 set as? 

Better yet, upload your IOC file.

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.
AHayee
Associate II

The issue is resolved after I added the following function

void SysTick_Handler(void){
	HAL_IncTick();
	HAL_SYSTICK_IRQHandler();
}

Thanks everyone for your support