2023-03-09 9:22 AM
2023-03-17 8:38 AM
Hello,
Thank you for bringing these typos to our attention and I reported internally.
Internal ticket number: 147877 (This is an internal tracking number and is not accessible or usable by customers).
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-09 10:08 AM
Hello @Community member ,
Thank you for reporting this typo.
I confirm that and I will check internally.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-09 10:20 AM
Thanks, Kaouthar.
Jan
2023-03-09 10:58 AM
Also at least for STMF0 and STMF4 (but maybe others), in RTC_ISR:
This register is write protected (except for RTC_ISR[13:8] bits).
Should be:
This register is write protected (except for RTC_ISR[15:8] bits).
2023-03-09 3:30 PM
That RTC_ISR thing is the same also for F7 and L4.
2023-03-10 2:32 AM
Wouldn't it be simpler to list the two bits which *are* write protected? :)
JW
2023-03-11 2:33 AM
Also for L0 and L1.
2023-03-11 2:39 AM
RTC_ISR[15:8] (full byte) is not write protected.
2023-03-13 3:36 AM
Hello,
Thank you for having reported the point.
I will check internally.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-17 8:38 AM
Hello,
Thank you for bringing these typos to our attention and I reported internally.
Internal ticket number: 147877 (This is an internal tracking number and is not accessible or usable by customers).
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.