cancel
Showing results for 
Search instead for 
Did you mean: 

the RM0090 reference manual for 2014 ,in the description of the “Chip Select togglest�? different from RM00990 reference manual for 2018,why?

cxiao.6
Associate II

the RM0090 reference manual for 2014 ,in the description of the “Chip Select togglest�? different from RM00990 reference manual for 2018,which one is correct?The results of our tests are consistent with reference manual for 2014,Is it wrong in RM00990 reference manual for 2018?

2018 version

0690X0000087VffQAE.bmp2014 version0690X0000087VfaQAE.bmp

8 REPLIES 8
cxiao.6
Associate II

anyone know?​

Imen.D
ST Employee

Hello,

We will check this internally and come back to you with clarification.

Kind Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Probably because RM0090 covers a broader range of parts, and that expanded over time, and also covers multiple die steppings where errata were addressed, or IP updated. Perhaps someone pointed out behaviour that was different to that described.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Imen.D
ST Employee

Hello,

The sentence in the RM0090 reference manual for STM32F4 (2018 version) is correct.

Can you precise which mode are you using ?

Kind Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Modul 1​

mode 1​

cxiao.6
Associate II

MODE 1