2023-03-07 9:44 AM
STM32L071CBT wakeup power button PC13, PWM signal = PA11
I have a device that wakes every 20 seconds then goes to sleep, it can also wake when the power button is pressed, part of it's wake cycle it to check the servoInt pin for activity.
pin setup
/*Configure GPIO pin : servoInt_Pin */
GPIO_InitStruct.Pin = servoInt_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING_FALLING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(servoInt_GPIO_Port, &GPIO_InitStruct);
/*Configure GPIO pin : powerButton_Pin */
GPIO_InitStruct.Pin = powerButton_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_InitStruct.Pull = GPIO_NOPULL;
HAL_GPIO_Init(powerButton_GPIO_Port, &GPIO_InitStruct);
stop mode is called
if(HAL_RTC_SetAlarm_IT(&hrtc, &RTC_AlarmStructure, RTC_FORMAT_BIN) != HAL_OK)
{
ErrorHandler(ERR_RTC_ALARM);
}
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
IRQHandler
void EXTI4_15_IRQHandler(void)
{
if(__HAL_GPIO_EXTI_GET_FLAG(servoInt_Pin) != RESET)
{
HAL_GPIO_EXTI_IRQHandler(servoInt_Pin);
}
else if(__HAL_GPIO_EXTI_GET_FLAG(powerButton_Pin) != RESET)
{
HAL_GPIO_EXTI_IRQHandler(powerButton_Pin);
}
callback handler
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
switch (GPIO_Pin)
{
case servoInt_Pin:
servoFlag = true;
break;
case powerButton_Pin:
powerTick = HAL_GetTick();
break;
}
}
the IRQ handler decerns the two exti lines and calls the callback correctly but the device wake on WFI from the servoInt_pin as well as the powerButton pin.
Is there a way to make WFI not be triggered from exti11?
Solved! Go to Solution.
2023-03-07 10:20 AM
Disable the EXTI11 interrupt before entering STOP mode, reenable upon exiting it in any way.
JW
2023-03-07 10:20 AM
Disable the EXTI11 interrupt before entering STOP mode, reenable upon exiting it in any way.
JW
2023-03-29 1:55 AM
Hello @markH
As Jan already said,
Add a line to disable the servoInt_Pin EXTI interrupt before entering stop mode:
HAL_NVIC_DisableIRQ(EXTI11_IRQn); // Disable EXTI11_IRQn to prevent waking up from servoInt_Pin
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
and then, add a line to re-enable the it after waking up from stop mode:
HAL_NVIC_EnableIRQ(EXTI11_IRQn); // Re-enable EXTI11_IRQn
after waking up from stop mode
With these changes, the device should only wake up when the power button is pressed while in stop mode.
You can also check this wiki article that provides steps and code for all the low power modes.
Hope that helps!
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-29 3:03 AM
In addition to what Jan and Sarra said, here is everything you have to learn and implement for the code to actually work:
https://community.st.com/s/question/0D53W00001nYvGgSAK/mc-sdk-not-work-with-mcu-stop-mode
Post edited to adhere community guidelines.
2023-03-29 4:12 AM
Thank you, waclawek.jan answer worked, I sort of realised on my way home after I posted the question. Sometimes you have to step back to allow yourself to think!