2025-08-11 4:07 PM
Hello.
I'm trying to launch a minimal LoRaWAN project. CubeMX version 6.15.0. When using MSI RC clocking, the module works without issues. When attempting to use the TCXO, the module starts, packets are successfully transmitted to the server, but are not received (IRQ_RX_TX_TIMEOUT error).
In the "LoRaWAN Middleware / TCXO Support" settings, it displays "TCXO not available," and no other options are present.
Part of the code from the SystemClock_Config initialization function:
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS_PWR;Attaching screenshots of the settings.
2025-08-12 5:32 AM
Hello @Zedder
There is issue related to reception will using the TCXO. For this error, i suggest you to increase the timeout used for reception.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.