cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 RM0399 Rev4 FDCAN Typos?

steezeman
Associate

Looks to me like the FDCAN peripheral has a few registers that are marked 'r' when they are likely 'rw' in the RM. They are the registers that configure the size of the FDCAN messages. This isn't blocking my work; only thought the ST team should know so they can fix it if it is indeed a typo.

 

Screenshot 2024-02-29 at 09.13.44.png

Screenshot 2024-02-29 at 09.13.55.png

1 ACCEPTED SOLUTION

Accepted Solutions
SofLit
ST Employee

Hello @steezeman ,

Welcome to the community and thank you for raising this issue.

I will escalate this issue internally to be fixed in the coming revisions of the RM.

Thanks again.

Internal Ticket 174976 for internal follow-up (not accessible by the community users).

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
SofLit
ST Employee

Hello @steezeman ,

Welcome to the community and thank you for raising this issue.

I will escalate this issue internally to be fixed in the coming revisions of the RM.

Thanks again.

Internal Ticket 174976 for internal follow-up (not accessible by the community users).

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.