cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H5 PSSI RDY pin setup and hold times verification

Hi,

STM32H533 datasheet (DS14539 Rev 2) in table 88 says that RDY input setup and hold time are both 0.5ns. From my naive point of view it looks like superb value (RDY have to be stable only +-0.5ns around CLK edge). Isn't that a typo ? (STM32H7 PSSIs hold time is about 5.5ns)

h5.png
Thanks,
Michal Dudka

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

After an internal check, all the values of H5 in the datasheet are correct while for H7R/S:

th(RDY) : the minimum RDY input hold time is 0ns and not 5.5ns.

New internal ticket for issue follow up on H7RS: 201229.

Thank your for your valuable contribution.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
mƎALLEm
ST Employee

Hello,

I'm checking internally if it's the same timing as STM32H7R/S product.

Most probably the issue is on "RDY input hold time" timing (need to check).

From STM32H7S datasheet:

SofLit_0-1737622809131.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
mƎALLEm
ST Employee

Hello,

After an internal check, all the values of H5 in the datasheet are correct while for H7R/S:

th(RDY) : the minimum RDY input hold time is 0ns and not 5.5ns.

New internal ticket for issue follow up on H7RS: 201229.

Thank your for your valuable contribution.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Great. Is this value verified by measurement? I have preliminary observations from which it seems that RDY signal deasserted during CLK edge (asserted 4.9ns after CLK edge) is interpreted as asserted. But I haven't tested it hard enough to say for sure. In a week or two, I might get back to you with that... unless I find a bug somewhere in my code.


@Michal Dudka wrote:

Great. Is this value verified by measurement? 


The values are provided by characterization:

SofLit_0-1737705664511.png

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.