Skip to main content
Associate II
Nov 12, 2024 8:34 AM UTC
Question

STM32H563 Warning: The Core is locked up

Hi,

I'm currently developing a custom application which provisions and regresses an STM32H563, using the NUCLEO-H563ZI board for development.

The CubeProgrammer CLI commands I'm executing are based on the bash scripts generated by CubeMX. Since I started playing around with those, somewhere the MCU got into a state which I can't get it out of.
Starting a Debug Session with a fully working Binary (tested on my 2nd Nucleo Board) results in an immediate HardFault. Breakpoint at Reset_Handler not even triggered. BFARValid == 1, BFAR = 0x2009fff0, contents of 0x2009fff0 unreadable.

In CubeProgrammer GUI, I can Halt the CPU immediately after resetting, showing a PC of 0x80034E0 (reset handler address), and when stepping one more time, PC = 0xEFFFFFFE.

When Downloading a Binary through the GUI, I get a warning "The Core is locked up". Full Connect&Download Output:

Spoiler
09:15:21 : Disconnected from device.
09:15:22 : UR connection mode is defined with the HWrst reset mode
09:15:22 : ST-LINK SN : 0032002B3132511238363431
09:15:22 : ST-LINK FW : V3J15M7
09:15:22 : Board : NUCLEO-H563ZI
09:15:22 : Voltage : 3.25V
09:15:22 : Warning: Connection to AP 0 requested and failed, Connection established with AP 1
09:15:22 : SWD freq : 8000 KHz
09:15:22 : Connect mode: Hot Plug
09:15:22 : Reset mode : Software reset
09:15:22 : Device ID : 0x484
09:15:22 : Revision ID : --
09:15:22 : Debug in Low Power mode enabled.
09:15:22 : SFSP Version: v2.5.0
09:15:22 : UPLOADING OPTION BYTES DATA ...
09:15:22 : Bank : 0x00
09:15:22 : Address : 0x40022050
09:15:22 : Size : 112 Bytes
09:15:22 : Bank : 0x01
09:15:22 : Address : 0x40022070
09:15:22 : Size : 16 Bytes
09:15:22 : Bank : 0x02
09:15:22 : Address : 0x40022080
09:15:22 : Size : 16 Bytes
09:15:22 : Bank : 0x03
09:15:22 : Address : 0x400220e0
09:15:22 : Size : 16 Bytes
09:15:22 : Bank : 0x04
09:15:22 : Address : 0x400221e0
09:15:22 : Size : 16 Bytes
09:15:22 : Bank : 0x05
09:15:22 : Address : 0x40022090
09:15:22 : Size : 8 Bytes
09:15:22 : Bank : 0x06
09:15:22 : Address : 0x400220f0
09:15:22 : Size : 8 Bytes
09:15:22 : Bank : 0x07
09:15:22 : Address : 0x400221f0
09:15:22 : Size : 8 Bytes
09:15:22 : Bank : 0x08
09:15:22 : Address : 0x400220f8
09:15:22 : Size : 8 Bytes
09:15:22 : Bank : 0x09
09:15:22 : Address : 0x400221f8
09:15:22 : Size : 8 Bytes
09:15:22 : UPLOADING ...
09:15:22 : Size : 1024 Bytes
09:15:22 : Address : 0x8000000
09:15:22 : Read progress:
09:15:22 : Data read successfully
09:15:22 : Time elapsed during the read operation is: 00:00:00.008
09:15:32 : Memory Programming ...
09:15:32 : Opening and parsing file: stm32h5-bootloader.bin
09:15:32 : File : stm32h5-bootloader.bin
09:15:32 : Size : 338.34 KB
09:15:32 : Address : 0x08000000
09:15:32 : Erasing memory corresponding to segment 0:
09:15:32 : Erasing internal memory sectors [0 42]
09:15:32 : Download in Progress:
09:15:33 : File download complete
09:15:33 : Time elapsed during download operation: 00:00:01.212
09:15:33 : Verifying ...
09:15:33 : Read progress:
09:15:34 : Download verified successfully
09:15:34 : RUNNING Program ...
09:15:34 : Address: : 0x08000000
09:15:34 : Warning: The core is locked up
09:15:34 : Start operation achieved successfully

The CLI Commands I used in my custom application are those (roughly from regression.sh):

STM32_Programmer_CLI -c port=SWD speed=fast ap=1 debugauth=3
STM32_Programmer_CLI -c port=SWD speed=fast ap=1 -hardRst -ob TZEN=0xC3
STM32_Programmer_CLI -c port=SWD speed=fast ap=1 -sdp ./DA_ConfigWithPassword.obk
STM32_Programmer_CLI -c port=SWD speed=fast ap=1 debugauth=1 per=a pwd=./password.bin

Which, in hindsight, I should have thought more thoroughly about, because they make little sense in my application (no TZ). I believe one of those commands triggered my issue. Unfortunately I cannot say for sure, because it took a while to realize the MCU was not running properly any more...

I tried resetting all the option bytes to their default values, but still experience the Core Lockup.
I also tried Provisioning, Closing and Debug-Authenticating the Device multiple times using the GUI, to no effect.
Other Posts with other STM32 Series MCUs (F, L, ...) describe the solution to move out of RDP, but I think this option byte was removed in the H(5) Series...

Is there a way to get out of this problem or did I brick my MCU completely?

Thanks in advance and best regards,
Stefan

This topic has been closed for replies.

2 replies

ST Employee
Jan 8, 2025 3:24 PM UTC

Hello @beartronics, sorry for the delayed answer

This issue gas been spotted and it is normally corrected with v2.18.0 released under st.com.

Could you confirm that? 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
Jan 21, 2025 1:00 PM UTC

Hello @Sarra.S ,

Thank you for the response.

I tried with 2.18.0, but get the same behaviour when downloading a working binary: "Warning: The core is locked up" and an immediate HardFault if I download the binary via CubeIDE..

It seems the "Register" View in CubeProgrammer GUI was completely overhauled, but still, in the bottom right corner I can see "CPU: LOCKUP".

So, upgrading to 2.18 was no solution.

Best regards,
Stefan